Configuring BBH SCU with AKD2G SRA parameters This article shows how to make a simple safety Application with KAS and SafePLC2. The Functional Safety parameters can be configured in WorkBench or in the BBH SafePLC2. Both methods are described here. |
jeeva |
English | |
AKM2G Standard Voltage and Low Voltage Winding Thermal Sensor OptionsA description of the thermal sensor options for the AKM2G Standard and Low Voltage series motors. | English | ||
AKD and the Raspberry PiRaspberry Pi Foundation and its background. The foundation's goal was to advance the Computer Science, Programming, and engineering education of children and adults with a low-cost and high-performance solution. From Raspberry Pi Foundation itself: | ArielM |
English | |
Configuring The AKD X9 EEO AS General Digital I/OThe X9 Port on the AKD drive is generally used as an encoder input, EEO (encoder emulated output), or not used. However, the AKD also has the feature to use the X9 port as general I/O. |
jcoleman02 |
English | |
S300, S700 ROFFSABS, Absolute Encoder Single TurnWhen configuring the S700 or S300, homing with an absolute encoder you will need to use ROFFSABS. ROFFSABS provides the necessary offset when physically homing. Single Turn Absolute is absolute to 1 rotation of the motor. | ArielM |
English | |
TwinCAT 3 To AKD2G EtherCAT Setup and DemonstrationThe attached video covers important topics such as ESI (XML) file acquisition and importation into TwinCAT 3. Basic setup and motion from the TwinCAT 3 console are also demonstrated. Finally how to recognize and resolve a mismatch between the Device Description (ESI) and the physic |
toddevans01 |
English | |
Reading of AKD axes position by Python and Raspberry Pi 3 Modell BThis solution allows you to read the motor positions of three AKD axes using Raspberry Pi hardware and Modbus TCP/IP. |
Stefano Giacomelli |
English | |
AKD2G Low Voltage DC Operation Table of Contents Overview | gby |
English | |
Mean Time Between Failure AKD AKM Gen 1Summary of Juran's Mean Time Between Failure (MTBF) for AKD & AKM. Data up through 2014. Purpose A rough calculation of the Mean Time Between Failure (MTBF) based on historical data. This tool is to be used at a customer's request. MTBF is not "operating life" or "service life". | JohnKeesee |
English |
Don't know if you need a servo or stepper?
Motor Windings: Understanding How They Work and Affect Performance
Read MoreEngineer the Exceptional
Learn More