RS232 and RS485 SpecificationsRS-422 drivers, receivers are unidirectional. | Ann Pater |
English | |
G & L Basic Support Document This document covers the basic support for the G&L products. It includes information on the three different edition levels of PicPro. Information on the different G&L files types and how to determine what version of firmware being used in the Smart Drives | English | ||
Resolving Servo Feedback ChoicesThis PowerPoint presentation explains the differences between different types of servo motor feedback devices, including: | English | ||
AKD2G EtherNet/IP Landing PageThe AKD2G Ethernet/IP Landing Page provides supplementary application notes related to AKD2G Ethernet IP. |
toddevans01 |
English | |
Cam Profile Build, Release, Switch Organization, FB for PLC Open. This article is related Cam Build & Release Organization. The attached file consists of a FB you may use in your project. In some machines, we need different cam profiles and we change these profiles for system expectations. |
Ezel |
English | |
AKD2G vs AKD Profinet ComparisonThis article contains a list of differences between AKD2G and AKD1G related to Profinet. |
jcoleman02 |
English | |
AKD Command Source for EtherCAT/CANopenThe AKD command source (DRV.CMDSOURCE) is set automatically by the EtherCAT/CANopen master controller. There is no need to set this in Workbench when using the fieldbus. And there is no need to read DRV.CMDSOURCE to verify that it's set correctly as long as there is nothing configured |
jcoleman02 |
English | |
Workbench loses connection when EtherCAT master is connected to the AKD using EoEEoE Overview EoE = Ethernet over EtherCAT |
jcoleman02 |
English | |
Getting Started with the AKD/AKD2G Performance Tuner (PST)This document reviews the basics of getting started with the PST (Performance Servo |
C Wontrop |
English |
Don't know if you need a servo or stepper?
Motor Windings: Understanding How They Work and Affect Performance
Read MoreEngineer the Exceptional
Learn More