AKD2G SYSTEM CONFIGURATION WITH KOLLMORGEN DDL LINEAR MOTORSThis document shows the wiring requirements for connecting the DDL linear motors to the AKD servo drive. It also describes the setup procedure for configuring the AKD2G drive in the Workbench software. |
toddevans01 |
English | |
AKD2G DS402 and Manufacturer Specific Torque and Current Setpoint and FeedbackFor AKD1G ECAT users the objects 2071h and 2077h do not exist. See the following app note for equivalents with the AKD2G ECAT drive. |
Will Gaffga |
English | |
S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition. If the axes group is travelling in a line at constant speed, the acceleration vector is zero… | Jeanie |
English | |
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos. |
Will Gaffga |
Portuguese, Brazil | |
Retrofit KAS EtherCAT Backups with AKD2G FirmwareThe AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier). The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of restoring the drive’s configuration once any AKD2G… | Jeanie |
English | |
AKD2G EtherCAT W7011 Warning and F7011 Fault Synchronization Error SupportThis article provides details related to cause and remedy of the W7011 warning and F7011 Fault in the AKD2G EtherCAT drive. |
toddevans01 |
English | |
Convert AKD-B Parameter File to AKD-PInstructions to convert a saved AKD-B parameter file into an AKD-P file to load into an AKD-P drive. |
Will Gaffga |
English | |
Using Siemens PD_TEL9_DrivePos with Telegram 9 for Positioning with AKD2G Profinet RTThis document provides test results when using Siemens PD_TEL9_DrivePos function block with AKD2G Profinet Telegram 9 |
Will Gaffga |
English | |
KAS v4.01 Software is now available!! KAS v4.01 Software is now available!! |
dusty.schafer |
English |
Don't know if you need a servo or stepper?
Motor Windings: Understanding How They Work and Affect Performance
Read MoreEngineer the Exceptional
Learn More