Skip to main content
blog | Meeting the ‘got milk?’ challenge in Europe's dairies |
|
2 minute read

Meeting the ‘got milk?’ challenge in Europe's dairies

Some years ago, a popular U.S. campaign reenergized the consumption of cow's milk. The "Got Milk?" campaign ran from October 1993 to February 2014 and has been accredited for greatly increasing California milk sales. In Sweden, heads were nodding at Europe's second largest diary company, Arla Foods; they knew they needed to "get milk" from production to storage in a more efficient manner.

In 2004, Arla Foods needed to make a decision. Their conveyor system was no longer up to the task of transporting dairy products from production to chilled storage. At the time, management decided to introduce manual warehouse trucks. Initially, Arla Foods operated five trucks two shifts a day for nearly four years; one truck was added later.

An active decision to improve efficiency

The decision to replace the six manual trucks with automated guided vehicles (AGVs) was made in 2009. The "new" trucks ran the same two shifts a day, now without operators. Two more AGVs were added later, and all eight were in use even as Arla Foods initiated the close of its Gothenburg, Sweden operations in 2013.

Relocating efficiency is easy

The new home of the eight AGVs was the Arla Foods dairy center in Falkenberg, Sweden. The ease of relocating to this facility demonstrated the versatility, expandability and flexibility of AGVs. Today, these eight machines function effortlessly, three shifts a day.

Expandability ensuring ROI

The introduction of AGVs in Arla Foods' operations in Götene, Sweden, is a prime example of AGV expandability. When management decided to employ the use of AGVs, they used a stepped approach. AGVs were introduced into different transportation processes in three steps. By the end of the project, a total of nine AGVs were installed; Arla Foods realized return on investment after two years.

Getting milk to 6M people

Finally, Arla Foods' distribution operations in the U.K. uses AGVs to move over 1.5 million liters of milk every day. In this custom-designed "refrigerator," 90+ state-of-the-art AGVs transport milk from the filling stations to dispatch, each one travelling more than 15km a day. This dairy delivers milk to nearly six million inhabitants in the counties of Greater Manchester, Somerset and West Midlands.

To find out more about how AGVs can meet your "got milk" challenges, speak with one of our automation specialists and read one of our success stories.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…