Skip to main content
blog | Eccentricity, Wobble, and How a Servo System Can Help |
|
2 minute read

By definition, Eccentricity is a measure of how much a roll deviates from being perfectly circular. Ideally, eccentricity should be zero, but in reality, it is never zero. Practically not a single roll is a perfect circle because it is produced using a machine which itself is prone to some machining errors (since it is product of some other machine and so on).

Eccentricity in the roll gives rise to wobble when rotated using a motor. Wobble is the angular deviation of the axis of rotation over one revolution.

Now let's understand how eccentricity can affect the machine performance.

Eccentric Roll Load Profile

Now consider two rolls in contact, one having half the diameter of the other.

Eccentric Rolls

With an induction motor, it expects to deliver a fixed torque at a fixed/constant speed. But as the load varies (due to eccentricity), the torque starts varying. The result is higher acceleration of the motor.

T = J x α (T - Torque, α - Angular Acceleration, J – Moment of Inertia)
Hence, α = T / J

So change in the torque gives rise to change in acceleration & hence change in speed.
If the motor is to deliver a fixed torque, then due to the load variation, the speed profile will be as shown below:

Eccentric Rolls Speed Profile

To maintain constant speed, the motor has to deliver torque as per the load variation.

Eccentric Rolls Torque Profile

Typically, the motor has to respond to changes in torque every 100 ms (e.g. for roll running at 600 rpm).Typically for induction motor, torque rise time is in the tune of 350-400 ms. So despite having superior drive control, a normal induction motor cannot respond in the required time frame. The more connected rolls, the greater the load variation. In production machines, there are many rolls rotating together at very high speeds.

How can Servo system help here?

1. Conventional systems driven by induction motors are not dynamic enough to respond to such quick changes (to the tune of 100 ms).
2. A permanent magnet synchronous servo motor (e.g. AKM from Kollmorgen) has torque rise times of 80-100 ms. Therefore, the response is faster.
3. A servo drive (e.g. AKD from Kollmorgen) has current controller cycle time of 670 ns (fastest in the industry) which helps the servo motor achieve the desired response.

 

Eccentric Rolls Servo Response


So in order to take care of varying torque demands due to eccentricity issues in the mechanical systems, servo based motion control systems can perform much better as compared to conventional systems. What kind of eccentricity issues have you had to deal with recently?

FAQ

  • Q: At what point should I consider upgrading from an induction motor to a servo system?

    A: If your process involves multiple rolls running at high speed — such as in printing, converting, or web-handling applications — and you're seeing speed inconsistencies, tension fluctuations, or product quality issues, eccentricity-related load variation is a likely culprit. A servo system becomes especially worthwhile when the number of connected rolls increases, since each additional roll compounds the total load variation that the drive must manage.

  • Q: Can a servo system compensate for eccentricity without mechanically correcting the rolls themselves?

    A: Yes — a servo system can effectively compensate for the torque and speed disturbances caused by eccentric rolls without requiring you to rework the mechanical components. By continuously adjusting current output to match real-time load demands, the servo drive absorbs the variation that the imperfect roll geometry introduces. That said, reducing eccentricity at the source through tighter machining tolerances is still good practice, as it reduces the corrective burden on the motion system.

  • Q. In what types of applications is controlling eccentricity wobble most important?

    A: Controlling eccentricity wobble is especially important in machines with multiple rotating rolls, such as printing, converting, packaging, and web-handling equipment. These systems operate at high speeds and rely on consistent motion control to maintain product quality. Using a servo system helps stabilize the process and reduce performance issues caused by mechanical imperfections

 

Consult an Expert

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Kollmorgen Essentials Motion Systems

Performance-matched. Value-Driven. Confidence included. Kollmorgen Essentials™ Motion Systems are ready to plug in, power up and perform.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When Should You Convert From a Stepper Motor to a Servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
Kollmorgen Essentials Family

Introducing Kollmorgen Essentials™ System for high-performance, affordable precision motion for every industrial axis  >

Simplify motion engineering, speed up setup and minimize costs. Kollmorgen Essentials™ Motion Systems are optimized for precision servo performance and value.​​
Functional Safety 101 White Paper

Functional Safety 101: The What, Why and How >

Mandates and regulations aside, more customers are demanding functional safety. But no two applications are exactly the same, and there isn’t a one-size-fits-all solution. This whitepaper reveals how equipment manufacturers can stay up to speed.
Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging

Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging >

Kollmorgen's expertise in motion control components for packaging machinery helped Packsize tackle demanding challenges to create game-changing packaging automation solutions.

Bandwidth, Gain and Phase Margin in Servo Systems: What is Phase Margin? >

Phase margin is a measurement in the frequency domain, taken from a Bode plot, that calculates the amount of phase lag above -180 degrees at the point on the amplitude plot that crosses 0dB (gain cross over frequency).

Five Motion Tips for Optimal High-Definition Metal Cutting Performance >

Achieve next-generation performance for laser, waterjet and plasma metal-cutting machines. Optimize the fieldbus, control loop bandwidth, servo motor design, feedback system and cabling using these 5 motion tips for high-precision metal cutting.

Motor Derating Due To High Ambient Temperatures >

How do I calculate a motor’s continuous torque when it is operating in an environment above its rated temperature? Since the motor’s continuous torque (Tc) is rated in a 40°C ambient, how can I estimate the motor’s continuous torque during my…