Skip to main content
Success Story | 2 minute read

Kollmorgen helps packaging automation provider meet the need for packaging

In recent years, e-commerce and global logistics have grown tremendously—with demand often outpacing capacity. Labor shortages, supply chain disruptions, increased competition and cries for sustainability further increase the pressure. Large retailers that ship a wide variety of products have found themselves at a crossroads: Find ways to innovate fulfillment and shipping processes or risk losing market share.

Challenge

Today’s consumer expects online orders to come quickly and conveniently—with enough packaging to protect their goods, but not so much as to create unnecessary waste and emissions. On the other hand, large retailers must accommodate massive order volumes and a seemingly endless range of product sizes, all while keeping labor, material and shipping costs down.

Packsize, a global leader in packaging automation solutions, sought to help answer this need. In March 2020, the company finished a prototype of its revolutionary X5®, the world’s first fully automated erected box system that delivers right-sized packaging on demand. Initial buzz was strong: Walmart expressed interest in the technology for its next-generation fulfillment centers.

This X5 evolution—dubbed the Ultra5—would have to be exceedingly reliable to meet Walmart’s uptime needs at its busy, mission-critical fulfillment centers. The pressure was on to scale production quickly and efficiently. All amidst a global pandemic and exploding e-commerce demand.

“To succeed with the Ultra5, we relied on Kollmorgen to deliver 1,000 components. Kollmorgen has established itself as a trusted partner in one of our core platforms and we expect their team to be a key part of that future success.” — Edwin Borrero, Packsize

Solution

When it came time to move to commercialization and full-scale production of the new packaging automation system, previous motion control partners fell just short of the project’s demanding requirements. The search was on for a partner who could deliver both technically and with a proven supply chain and a global footprint. Kollmorgen and its Swedish-based partner SDT delivered with the industry-leading 2G Motion System.

The hallmark of the 2G Motion System is its ability to deliver unrivaled performance and torque density in a compact package. In fact, AKM2G servo motors deliver an average of 30% greater torque density than previous generations with no change in package size or mounting, allowing for a reduced machine footprint without sacrificing performance. The AKD2G drive further reduces space requirements and bill of materials thanks to a single-cable connection, dual-axis drives and optimized smart features. This is a key benefit of motion control components for packaging machinery as it allows for more compact equipment design.

What’s more, the AKD2G drive enables a much easier and higher level of customization than competitive products—which ultimately allowed Packsize to enhance the Ultra5’s functionality and user experience. In addition to checking the technical boxes, Packsize chose Kollmorgen for its proven reputation—both in terms of product integrity and supply-chain reliability.

Kollmorgen 2G Motion System

Results

Even amid COVID-induced supply-chain snags, Kollmorgen and SDT delivered over 1,000 components to enable the shipment of 200+ X5/Ultra5 packaging automation systems globally within a single year of the product’s launch.

Walmart and other customers use the system to produce up to 600 custom-sized boxes per hour, each with up to 2 labels applied—the highest packaging throughput in its class. This right-sized approach to packaging contributes to lower labor and packaging costs, less waste, and fewer emissions. In fact, retailers who use the system can fit up to 33% more boxes on freight and delivery carriers.

If its retail customers are happy, so is Packsize. The company is taking advantage of continued growth and new product development opportunities—with its trusted motion partner Kollmorgen by its side.

600 custom-sized boxes per hour

Download as PDF

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.

Learn More

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.

How Cosmopack moved from specialized to flexible packaging solutions >

Learn how Cosmopack upgraded automated packaging line integration with decentralized motion architecture for more flexible packaging solutions.
Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever  >

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
Kollmorgen Essentials Family

Introducing Kollmorgen Essentials™ System for high-performance, affordable precision motion for every industrial axis  >

Simplify motion engineering, speed up setup and minimize costs. Kollmorgen Essentials™ Motion Systems are optimized for precision servo performance and value.​​
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…