Skip to main content
press_release | Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments |
|
minute read

bottling application

Radford, VA. — Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments. Kollmorgen Essentials Drive was designed with simplicity and flexibility in mind for fast commissioning and reliable performance at a value-driven price. By pairing KED with AKMA aluminum washdown motors and AKMH stainless-steel hygienic servo motors, machine builders can now achieve high-performance motion in demanding washdown applications—without the cost typically associated with washdown and hygienic servo systems.

Kollmorgen Essentials servo drives support multiple industrial Ethernet protocols out of the box, including EtherCAT®, EtherNet/IP™ and PROFINET®, providing broad connectivity while reducing system and inventory complexity.  

Cost-effective Absolute Feedback for Washdown Applications 

To further extend this value, AKMA and AKMH motors are now available with SFD-M (Smart Feedback Device, Multi-Turn), enabling Kollmorgen Essentials servo drives to support absolute multi-turn positioning in hygienic and washdown.

SFD-M delivers high-resolution absolute feedback without the cost and maintenance associated with battery-backed encoders. Its energy harvesting technology stores position information through power cycles, while embedded motor data enables automatic drive configuration and faster commissioning with all Kollmorgen servo drives, including KED, AKD® and AKD2G.

“High resolution, absolute multiturn feedback has traditionally required stepping up to a higher-cost servo system,” said Chris Cooper, Global Director, Product Management. “By integrating SFD-M into our AKMA and AKMH motors for use with the Kollmorgen Essentials Servo Drive, we’re delivering that same precision and control in a cost-effective solution designed for food and beverage, pharmaceutical packaging and other washdown applications.” 

Designed for Washdown and Hygienic Environments 

AKMA motors feature anodized aluminum housings with IP69K protection for medium to heavy-washdown applications. AKMH motors provide stainless steel construction with IP69K sealing for daily washdown environments involving high pressure, elevated temperatures and caustic cleaning agents.

With SFD-M available across these extended motor families, Kollmorgen delivers a unified 24-bit absolute feedback solution that provides consistent precision across a wide range of environments. Combined with Kollmorgen Essentials servo drives, machine builders gain high-performance, affordable motion solutions they can rely on for washdown and hygienic applications. 

About Kollmorgen  

Kollmorgen Corporation, a Regal Rexnord™ brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, AGV control solutions and automation control platforms. We deliver breakthrough solutions that combine exceptional performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.  

The following are believed to be the trademark and/or trade names of their respective owners and are not owned or controlled by Regal Rexnord Corporation: EtherCAT® (Beckhoff Automation GmbH); EtherNet/IP™ (ODVA, Inc.); PROFINET® (PROFIBUS Nutzerorganisation e.V.).

Regal Rexnord is a trademark of Regal Rexnord Corporation. 

Kollmorgen Essentials Motion Systems

Performance-matched. Value-Driven. Confidence included. Kollmorgen Essentials™ Motion Systems are ready to plug in, power up and perform.
Learn More

Kollmorgen Essentials Servo Drive

Flexibility AND features. With Essentials, you get 3 major industrial Ethernet protocol options in one drive, plus features not often seen in value-based drives.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

cost-optimized motion control

Reliable, Cost-Optimized Motion Control for Food Processing Washdown Applications >

Join this live webinar to discover how Kollmorgen Essentials™ Servo Drives (KED) paired with AKMA washdown motors and AKMH hygienic stainless‑steel motors deliver high‑performance, washdown‑ready motion across food contact, splash‑zone, and non‑food…
English, UK

Enhancing Washdown Motor Performance with a Unified, Cost-Optimized Motion Control System >

In this webinar, you’ll discover how the Kollmorgen Essentials™ Servo Drive (KED), combined with IP69K-rated AKMA anodized aluminum and AKMH stainless-steel servo motors, deliver reliable, high-performance motion at a value-driven price.
Kollmorgen Essentials Servo Drive Datasheet

Kollmorgen Essentials Servo Drive Datasheet >

The servo drive with built-in features for faster commissioning and proven reliability at an exceptional value.
Kollmorgen Essentials Selection Guide

Kollmorgen Essentials Catalog >

Modern motion control success begins with robust, flexible and value-driven systems that allow you to get your machine designs to market quickly. The new Kollmorgen Essentials™ Motion System is engineered to help machine designers meetmost motion and…
Kollmorgen Essentials™ Motion Systems Brochure

Kollmorgen Essentials™ Motion Systems Brochure >

Learn more about the new Kollmorgen Essentials Motion System — designed for value, ease, scale and performance.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

How can food packaging machine builders meet stricter food safety rules without sacrificing OEE? >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.
Kollmorgen AKMA Anodized Washdown Motor Catalog

AKMA Anodized Washdown Motor Catalog >

AKMA servo motors from Kollmorgen are designed for critical medium to heavy washdown environments and variable weather applications. These lightweight, workhorse motors incorporate a hardened anodized aluminum coating, a versatile form factor, and…