Skip to main content
press_release | Kollmorgen introduces the AKMA servo motor to meet the demands of medium- to heavy-washdown applications |
|
minute read

Kollmorgen AKMA motor

RADFORD, VA.,  — Kollmorgen, a global leader in high-performance motion control systems, today announced the launch of its AKMA servo motor built specifically for durability, cleanability, and versatility. The motor employs a hardened anodized aluminum surface to offer machine designers a cost-effective hygienic option to stainless steel in medium- to heavy-washdown applications.

The lightweight design of the AKMA motor makes it easy to install and maintain, and its high torque density offers machine builders more performance in a smaller footprint. The motor is ideally suited for precision motion applications in food & beverage processing, and in pharmaceutical & medical packaging operations. The AKMA’s IP69k rating enables it to deliver high performance even in wet and rugged environments, supporting critical applications like tracking and positioning for antenna pedestal systems.

An anodized aluminum surface offers strong resistance to chemicals across a wide pH range. Since the motor’s smoother and hardened surface is more scratch resistant and will not flake like a painted motor, it can be used above the food line. The AKMA’s stainless steel shaft meets functional safety requirements, while its “one-piece” rounded housing structure eliminates the need for a seal between the flange and housing to prevent puddling and water ingress. The AKMA motor also features a vented design to equalize pressure inside and outside for increased OEE and motor durability.

“We are excited to offer the AKMA servo motors to engineers searching for an affordable motor choice in wash-down environments where stainless steel surfaces are not necessarily required,” said Ross McMillan, Vice President of Engineering at Kollmorgen. “Now, it’s possible to balance performance with value and avoid overspending for a surface quality you may not need.”

For more information, visit https://www.kollmorgen.com/en-us/products/motors/servo/akma

About Kollmorgen

Kollmorgen, a Regal Rexnord brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, linear actuators, AGV (Automated Guided Vehicle) control solutions, and automation control platforms. We deliver breakthrough solutions that combine exceptional performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure washdowns are essential to keep machines free from pathogens, yet these washdowns are often incomplete, ineffective and damaging to motors and other equipment. Common practices such as shielding or bagging motors to prevent damage are extremely time-consuming. Direct washdown of equipment that is not properly designed to prevent water ingress can lead to premature failure. Irregular and rough surfaces can harbor pathogens that are difficult to remove. Eliminate all these issues by employing these best practices for the design of a more hygienic and productive machine.
Learn More

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

cost-optimized motion control

Reliable, Cost-Optimized Motion Control for Food Processing Washdown Applications >

Join this live webinar to discover how Kollmorgen Essentials™ Servo Drives (KED) paired with AKMA washdown motors and AKMH hygienic stainless‑steel motors deliver high‑performance, washdown‑ready motion across food contact, splash‑zone, and non‑food…
English, UK
Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments

Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments >

Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments.

Enhancing Washdown Motor Performance with a Unified, Cost-Optimized Motion Control System >

In this webinar, you’ll discover how the Kollmorgen Essentials™ Servo Drive (KED), combined with IP69K-rated AKMA anodized aluminum and AKMH stainless-steel servo motors, deliver reliable, high-performance motion at a value-driven price.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

How can food packaging machine builders meet stricter food safety rules without sacrificing OEE? >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.
Kollmorgen AKMA Anodized Washdown Motor Catalog

AKMA Anodized Washdown Motor Catalog >

AKMA servo motors from Kollmorgen are designed for critical medium to heavy washdown environments and variable weather applications. These lightweight, workhorse motors incorporate a hardened anodized aluminum coating, a versatile form factor, and…
AKMA Servo Motor in washdown

Bringing Performance and Reliability to Harsh Environments with Lightweight AKMA Motors >

Learn how lightweight Kollmorgen AKMA servo motors deliver durability, cleanability and performance in medium and heavy washdown applications.
AKMA Servo Motor Brochure

AKMA Servo Motor Brochure >

The AKMA servo motor features durability, cleanability and versatility for medium to heavy washdown applications.