(ABD & ABM) Altra Brasil Servo SeriesAs séries ABD® (Altra Brasil Drive) e ABM® (Altra Brasil Motor) oferecem uma linha completa de servo-acionamentos com base nas tecnologias EtherCAT e Analógico, desenvolvida sob medida para atender às demandas do mercado brasileiro.
AKD EtherCAT Scaling for Velocity, Acceleration, and DecelerationThis article discusses AKD EtherCAT scaling for velocity, acceleration, and deceleration commands and actual velocity. For the position modes, FBUS.PARAM05 applies to position scaling and the scaling for velocity, acceleration, and deceleration.
inglês
AKD EtherCAT Flexible PDO Mapping Size Limitations and PaddingThe AKD drive supports flexible EtherCAT PDO mapping. The 4 available flexible RxPDO’s (PDO data for receive direction, commands from master to drive) are mapped using objects 1600h, 1601h, 1602h, and 1603h. Each one of these RxPDOs is limited to a maximum size of 8 bytes, but…
AKD Profinet PN.ACCSCALING ExamplesPN.ACCSCALING sets the scaling factor for acceleration rates related to PROFINET motion commands.
The AKD PROFINET manual states that it applies to Jog Acc (PNU 1006), Jog Dec (PNU 1007), DRV_ACC (Telegram Signal 108), and DRV_DEC (Telegram Signal 109), and no other parameters.
However…
inglês
Getting Started with PxMM UDP Communications - using Packet SenderThis application note uses the PC utility Packet Sender (download at https://packetsender.com/) to perform simple communications between a PxMM and a PC. The program “udpProgram” in the project UDP test Send-Receive First Transmission Each Way.kas has been added to a .kas…
inglês
MLFB_HomeFindHomeInput with additional featuresThe KAS IDE comes with the UDFB (User-Defined Function Block) MLFB_HomeFindHomeInput. This post contains an updated version of the UDFB with the following changes:
The homing sensor was used as normal detection, It is set to detect falling edge.
After the home sensor is tripped…