Search Articles
| Modify old Profinet configuration done with KAS 2.7Problem When you open a project created with KAS 2.7 in a newer KAS release, you could have an error message when you try to open the PDMM Profinet device configuration in the fieldbus editor: "K5BusPNIODev - Invalid or corrupted configuration file" | inglês | |
| Protocols Supported by AKD DriveCurrent general market model numbers and their supported protocols | inglês | |
| KAS IDE Crashes On StartupDoes KAS IDE crash on your system before displaying the splash screen, displaying this instead: | inglês | |
| Division by Zero in PLC ProgramsWhen debugging a program in KAS, you may run into a situation where there is a division by zero. These errors can be challenging to locate. The solution is to have an exception routine for this condition. | inglês | |
| Reading the Status of Inputs for AKD CANOpenFor reading the Input status, State, for the Digital Inputs 1 – 7 on the AKD drive the object is 60FDh for digital inputs. This is defined by the standard DS402. | inglês | |
| S700 Safety: Safely limited speed Table of Contents General Example Applic | inglês | |
| RDP GeneralValid for S700 / S300 For configuration of RDP functionality see RDP - Rack Drive panel | inglês | |
| Setup of an Endat or Hiperface or BISS encoder Valid for S300, S400, S600, S700 | inglês | |
| Data storage in Endat or Hiperface or BISS encoders Valid for S300, S400, S600, S700 | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >