Skip to main content
Success Story | 2 minute read

Safety via Slip Ring

Safe Torque Off: Kollmorgen and Stemmann-Technik are developing a TÜV-certified solution

Safe Torque Off (STO) in practice
Safe Torque Off (STO) in practice: a Swiss manufacturer of test equipment is already using the TÜV-certified safety technology based on a slip ring and AKD-N servo drives from KOLLMORGEN arranged in a distributed setup.

Slip rings emerged at the same time as electric motors and generators. The operating principle, which involves sliding contacts on rotating circular conductors, is essentially fairly simple. Any issues relate to matters of detail, and these are the things that currently present the main challenge to developers – with regard, for example, to the growing role of safety technology in the field of engineering. For one thing, it is not that easy to transfer data, energy, air, or fluids from a static location to a component in constant rotation. The motion control experts at Kollmorgen have now managed, together with the slip ring manufacturer Stemmann-Technik, to develop a TÜV-certified safety solution – with UL approval – for this kind of thing.

Rotary indexing tables are a common piece of equipment used in an assembly and test stand context. Various work stations are arranged around an outer radius and take the component, held in a workpiece carrier, through another production stage with each indexing operation. If the workpieces on the rotating table still require rotational or linear positioning as well, the drives need to move as well. The job of slip ring systems is to transfer the power required for this along with the relevant control data. This is an established technology and works reliably well throughout a long service life. Things really get exciting, however, when this kind of slip ring is used to transfer safety-related data too. This was the task facing Kollmorgen as part of a project for a manufacturer of measurement inspection machines, with the aim being to investigate the behavior of crystalline components.

Benefits of distributed servo technology

The idea behind the engineering project was to install not only the actuators but also the controls on the rotary indexing table – adopting a distributed arrangement to save space. The Kollmorgen solution to this task was to use AKD-N servo drives, in a distributed setup, and compact AKM synchronous servo motors with high power density. The main benefits of the distributed setup and of having just one cable connecting drive and motor are small control cabinets and the fact that less space is required for installation purposes. In addition, the single cable connection technology, with the option to loop from drive to drive, also improved the inertia of the rotary indexing table. But it was still necessary to satisfy the safety technology requirements. This is integrated into the test station in the central AKD-C power supply module, which means a connection to the servo axes is required.

The Safe Torque Off (STO) feature was needed because the masses being moved – the rotary indexing table has a diameter of 120 cm after all – present a potential hazard to persons in the vicinity. The testing process does, however, envisage some operator intervention on the system, which ultimately implies Safe Torque Off as regards evaluating safety.

The central AKD-C power supply module does in fact feature STO as standard – albeit connected to clearly defined and certified cables. Using a slip ring as a connecting element between the central AKD-C power supply module and the AKD-N drives would inevitably mean disconnecting the cable, however, and invalidate certification. The same also applies to any existing UL approval. This too would no longer be effective.

Safety in the slip ring – with a certificate

As part of the joint engineering project with the test stand builder, Kollmorgen began to look for a suitable manufacturer of slip rings who would be willing and able, together with the servo drive and motion control specialists, to develop a safety slip ring with TÜV certification. The current solution, approved by TÜV Süd, is based on a slip ring from the Bako LP range from Stemmann-Technik. Compared with conventional slip rings, this transmission system (made in the German town of Schüttorf) offers a wide range of potential solutions for customized production – thanks to the numerous options available – along with UL approval.

The challenges associated the project included how to deal reliably, from a safety perspective, with the natural wear experienced by the contacts. In this regard, Stemmann-Technik would point out the reliable service life based on 35 million revolutions at maximum speeds of up to 80 rpm. Another challenging task was how to transmit safety signals reliably without interference. It should be noted here that the shielding integrated into the cables is no longer present in the slip ring. This then makes it necessary to find ways of preventing signaling errors caused by the coupling of interference signals.

Interference-resistant communication of signals

Kollmorgen and Stemmann-Technik are able to combat the familiar problems associated with EMC through two separate measures. From a design perspective, two shielded junction boxes in the safety slip ring interrupt the Ethercat communication supply via which the superimposed safety signal is transmitted. This ensures in particular that the magnetic influences from harmonics in the power wires do not cause any signal interference. The second aspect for ensuring high resistance to interference within the slip ring relates to the structure of the safety signals. Compared with the standard practice of arranging STO with 5 or 24 VDC signals, Kollmorgen uses AC signals with specific frequency patterns between the AKD-C, as the central module, and the distributed AKD-N servo drives.

In practice, this particular detail ensures that potential interference signals from the drive are completely ignored if they do not have the exact same frequency. This approach is therefore far more robust against interference – which ultimately, combined with the two separate junction boxes for power and signals, helped secure certification from TÜV Süd. Thanks to this equipment, engineering firms have the benefit of safely switching off the rotary indexing table without losing access to the positioning drives (which are also moving) for the workpiece carriers. Users also retain full access to all drives in the event of an emergency stop – which ultimately saves on time-consuming referencing as a result of undefined statuses.

Conclusion

The new safety slip ring solution, developed jointly by Kollmorgen and Stemmann-Technik, means users do not have to miss out on the benefits of drive-based safety technology. Even for applications involving slip rings. So certification of STO in the slip ring paves the way for streamlined solutions for incorporating Safe Torque Off into applications involving rotation – including with innovative single-cable connection technology and servo drives arranged in a distributed setup. And as far as the US market is concerned, this solution would also retain UL certification.

Author: Felix Haunschild, Safety Development, Kollmorgen Europe, Ratingen

 

ABOUT KOLLMORGEN

Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. For further information please contact [email protected] or visit our website www.kollmorgen.com

Download as PDF
AKM servo motors are compact and quick to install thanks in part to single-cable connection technology.

AKM servo motors are compact and quick to install thanks in part to single-cable connection technology.

The combination of STO and single-cable connection enables streamlined installation with AKD-N servo drives from KOLLMORGEN arranged in a distributed setup.

The combination of STO and single-cable connection enables streamlined installation with AKD-N servo drives from KOLLMORGEN arranged in a distributed setup.

Safe Torque Off (STO) is increasingly becoming the norm in the field of drive technology.

Safe Torque Off (STO) is increasingly becoming the norm in the field of drive technology.

The safety solution, certified by TÜV Süd, is based on a slip ring from Stemmann-Technik.

The safety solution, certified by TÜV Süd, is based on a slip ring from Stemmann-Technik.

Author: Felix Haunschild, Safety Development, Kollmorgen Europe, Ratingen

Author: Felix Haunschild, Safety Development, Kollmorgen Europe, Ratingen

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Direct Drive Motors Improve Flexographic Printing Performance

Recent work done by Kollmorgen—a global leader in manufacturing motor and motion solutions—has shown that it is possible to synchronize components within the flexo printing process without mechanical transmission by using closed loop control technology. This synchronization is key to managing web tension throughout the process while ensuring a steady repeat length.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

How Cosmopack moved from specialized to flexible packaging solutions >

Learn how Cosmopack upgraded automated packaging line integration with decentralized motion architecture for more flexible packaging solutions.
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen Helps Salvagnini Build More Energy-Efficient Metal-Bending Machines >

Innovation, competency, service. Through 60 years in business, these three commitments have helped the Salvagnini Group achieve global leadership in the field of sheet-metal processing equipment. As the #1 worldwide supplier of panel benders, and one…

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >

The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…

Stop, hold and go safely: Motion tuning for vertical loads >

When designing motion for applications such as vertical gantries and hoists, you need to take special care to ensure operator safety and operational efficiency. Let’s discuss best practices for meeting the particular challenges involved.

What are the Five Major Components of a Brushless Servo Motor >

Servo motors are used in numerous markets to power machines, instruments, robots, and other factory automation applications. This blog addresses five major elements of a conventional brushless DC servo motor: the rotor, stator, bearings, feedback and…
What is a closed-loop system?

What is a Closed-Loop System? >

When learning about servo motors and servo systems, you’re likely to encounter the phrase “closed-loop system.” If you’ve ever wondered what that means and how it works, you’ve come to the right place. Let’s step through some of the most common…