Skip to main content
Success Story | 2 minute read

Accelerating the Development of Next-Generation Prostheses and Exoskeletons

Humotech was founded in 2015 on one simple question: Instead of building prototype after prototype, what if engineers could evaluate the design of prostheses, orthotics, exoskeletons and other wearable machine concepts by programming a robot to emulate them in real time while a user walked?

Challenge

The Humotech Caplex™ testbed platform is a modular system used throughout the U.S, Canada and Europe in single-axis and multi-axis applications that aim to optimize biomechanical motion in wearable robots for people of widely varying needs and body types. Given the broad scope of applications, high-performance, versatile motion is essential.

Caplex systems precisely activate multiple Bowden cables to stabllize motion across multiple degrees of freedom in response to unpredictable human movements. Actuation is controlled by up to five servo motors, and units can be daisy-chained together to accommodate all the axes any application may require. Forces are high, rapid bursts of velocity are required, and servo loops must respond within milliseconds. Only the highest-performing servo motors and drives would suffice.

The first Caplex systems used motors from a Kollmorgen competitor, but Humotech wanted to achieve higher performance, lower acoustic and electrical noise, and more responsive control.

“Users of the Caplex system require upwards of 100 Nm applied very precisely and rapidly, with torque/speed response within milliseconds, to replicate human motion in prosthetic and exoskeleton applications. Kollmorgen has enabled us to exceed expectations with our actuator units thanks to the AKM and AKD products. We’re grateful for the opportunity to work together.”
—Josh Caputo, President & CEO, Humotech

Solution

In collaboration with a Kollmorgen solution partner, Humotech selected AKD servo drives and AKM servo motors for integration into its wheeled, floor-standing Caplex units. A high-performance EtherCAT field bus is used for communication within Caplex systems and between daisychained units that provide as many as 10 or more axes of motion.

With the torque, speed and versatility of Kollmorgen servo motion, modular Caplex systems can easily be tailored to the needs of each project — including healthcare, rehabilitation, defense, consumer sports, wellness, healthy aging and other applications — with minimal custom engineering.

Image 1

Results

The servo performance is impressive, exceeding expectations. AKM servo motors deliver up to 2,420 rpm and 125 Nm torque, driving a maximum cable speed of 4.3 m/s and maximum cable force of 6.58 kN.

Kollmorgen AKD drives receive commands from an external controller hundreds or thousands of times per second based on a desired joint response, and the AKM motors respond with the appropriate speed and torque faster than the human nervous system can achieve. Actuators are quiet, efficient, easy to use, reliable and safe.

Caplex systems have been proven in more than 8 years of operation, and Humotech continues to refine and expand the system to serve more customers and applications.

Image 2

Featured Products

AKM servo motors offer outstanding torque density and precision in the industry’s largest selection of standard servo motors and modifications for an ideal application fit.

AKD servo drives offer industry-leading performance, communication options and power levels in a compact footprint.

Image 3

About Kollmorgen

Kollmorgen, a Regal Rexnord Brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, AGV control solutions and automation platforms. We deliver breakthrough solutions that are unmatched in performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Download as PDF

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.