Skip to main content
Success Story | 2 minute read

Cosmopack application

As food and beverage lines get faster and more varied, secondary packaging grows more complex. Speed increases. Space shrinks. Cleaning becomes critical. Cosmopack builds the machines that perform in this reality. 

With more than 5,000 labeling, handling and packaging systems installed  worldwide, the company has deep experience across global production lines. For years, it has relied on specialized machines for each packaging format, from cardboard and film to flat or die-cut pads. While that model worked, it limited flexibility and added complexity to production lines. Cosmopack set out to change that and become a custom flexible packaging manufacturer.

“We are extremely satisfied with the collaboration and the Kollmorgen product range, which has demonstrated speed, reliability, and consistent performance. We will certainly consider Kollmorgen’s portfolio for future projects.”

—Eng. Simone Colombarini, CEO

CosmoPack

Challenge

The goal was simple yet ambitious. Have a single architecture that can handle different materials and formats while simplifying automated packaging line integration. This universal COMBI platform would replace older single-purpose models to serve a wider range of customers and products. 

The machines had to fit into compressed food and beverage lines, including applications such as vegetable oils, cheese trays or canned products in oil. These environments demand clean machine edges, simplified cabling and easy washdown access. Optional modules also provided the flexibility to configure machines for different production lines and add later without major redesign. Finally, the electrical cabinet had to shrink while supporting more axes and functionality. 

Timing was another constraint. Cosmopack needed a motion architecture that could be commissioned quickly, integrated reliably and reused across multiple machine configurations to keep production lines on tight schedules.

Solution

The answer was a decentralized motion architecture built around Kollmorgen’s AKD-N servo drives and AKD-C power supply. By mounting intelligence closer to the motors on the machine and centralizing only the power, the system reduced cabinet size and shortened cable runs. This created cleaner, more organized wiring along the machine perimeter and fewer components inside the control cabinet.

Decentralization also simplified installation and accelerated setup because much of the drive configuration was performed directly at the machine rather than through complex cabinet wiring, reducing time and costs. Automated packaging line integration was faster and more predictable. 

Kollmorgen supported Cosmopack with product training, axis configuration in CODESYS and EtherCAT communication setup. The engineer-to-engineer support helped the first machine reach production faster than previous projects.

Results

The benefits of Kollmorgen’s decentralized motion architecture were proven after the first COMBI installation. Beyond the smaller cabinets, cleaner machine edges and faster startups, commissioning time dropped significantly.

In operation, machines can coordinate up to 30 axes and achieve up to 80 cycles per minute per track, depending on the format. Even during peak season, with machines operating on a three‑shift schedule, the system maintains high performance and smooth, reliable operation—processing more than 500,000 packages with no unplanned downtime. 

The real achievement is the flexibility and consistency across packaging styles, from bottles and jars to trays and specialty containers. The flexible packaging system performs reliably with difficult shapes that are common in food and beverage lines, while remaining easy to clean and service. 

Building on the success, Cosmopack is adopting the same decentralized motion architecture for a legacy mixer machine and future project designs. More importantly, Cosmopack knows it has a motion platform and partner it can trust to deliver.

CosmoPack application and stats

Download as PDF

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure washdowns are essential to keep machines free from pathogens, yet these washdowns are often incomplete, ineffective and damaging to motors and other equipment. Common practices such as shielding or bagging motors to prevent damage are extremely time-consuming. Direct washdown of equipment that is not properly designed to prevent water ingress can lead to premature failure. Irregular and rough surfaces can harbor pathogens that are difficult to remove. Eliminate all these issues by employing these best practices for the design of a more hygienic and productive machine.
Learn More

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Kollmorgen Automation Suite Brochure

Kollmorgen Automation Suite Brochure >

Premier machine automation programming package for high-performance motion and control in minutes
Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging

Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging >

Kollmorgen's expertise in motion control components for packaging machinery helped Packsize tackle demanding challenges to create game-changing packaging automation solutions.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

Ask The Experts: Motion Control for Food Packaging  >

When you have questions about motion control, turn to Kollmorgen for expert advice. Our Ask the Experts series brings together skilled motion specialists to explore our customers’ most-asked questions and provide proven solutions.

Kollmorgen Helps Salvagnini Build More Energy-Efficient Metal-Bending Machines >

Innovation, competency, service. Through 60 years in business, these three commitments have helped the Salvagnini Group achieve global leadership in the field of sheet-metal processing equipment. As the #1 worldwide supplier of panel benders, and one…
Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production >

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Kollmorgen Automation Suite injects some pace into metalworking

Pipes cut to order >

Cut to length in no time at all, with no shavings and hardly any burs: Kollmorgen Automation Suite injects some pace into metalworking
KOLLMORGEN FREYMATIC LeanCut Machine Brick Industry

Bricks that can put in an appearance >

Motion Control by KOLLMORGEN makes fast and precise cuts from the column of clay