Skip to main content
Success Story | 2 minute read

DECENTRALIZED SERVO SOLUTIONS FOR METAL

Distributed servo technology bends panels into better shape

Salvagnini simplifies the design of its machines using drive solutions from Kollmorgen

 Kollmorgen Salvagnini Application

Making a departure from traditional drive architectures in its new P2lean generation of machines, Salvagnini the world's leading manufacturer of panel bending machines is using distributed servo amplifiers for positioning, instead of keeping drives installed centrally in the control cabinet. And with this solution, the new Kollmorgen AKD-N series generates cost savings throughout the whole value chain. Another first by the Italian machinery manufacturer: Replacing the central hydraulic pump by a synchronized network of electrically-driven servo actuators.

Kollmorgen SalvagniniEach bending machine process cycle starts by the operator laying a metal sheet on the horizontal work surface. The workpiece is aligned to the bending unit fully automatically, by positioning axes under a blankholder. This clamps the panel in place while the bending unit, with its moveable blades, quickly performs any number of upward or downward bends. The precision of the reference position is essential for subsequent manufacturing quality because it is only done once for each workpiece during the processing cycle.
 

Drives simply placed next to the motors

To drive the built-in positioning units, Salvagnini uses distributed AKD-N series servos from Kollmorgen. With the new product generation, from the drive technology and motion control specialist, it is very easy to install the drives directly where they are required, in close proximity to the motors. One advantage of this distributed architecture comes from the dramatically reduced cost of the cabling for the seven distributed servo axes in the P2lean. Using a central structure with control cabinet converters, the shielded cable between the motor and the drive and the cable for the feedback system previously could have needed laying up to 10 meters of cable. For the seven positioning axes that would have made a total of 140 meters of wiring (14 wires of 10 meters each). Kollmorgen Salvagnini World PremiereWith this solution, using a central AKD-C power supply module in the control cabinet and seven distributed servo drives in two groups with three and four axes, this has now been reduced to only 40 meters. The total length is calculated as follows: two hybrid cables with power supply and feedback between the power supply module and the two nearest drive cables for a total of 20 meters, plus three meters for connecting the three axes in the first group and four and a half meters for a further three axes in the second group, knowing that the average distance between the IP67 devices in the system is not more than one and a half meters. The power supply to the motors then has to be considered. They are also installed not more than one and a half meters from the distributed AKD-N servo drives. Because the Kollmorgen solution is equipped with its innovative single cable connection technology, only 7.5 meters more cable is needed. Considering only the use of the distributed AKD-N servo drives combined with the single cable connection system, this saves 100 meters of cable - by reducing from 140 to 40 meters or roughly 71%.  

More efficiency by using less

This careful management of equipment resources produces other improvements that are a direct result of having much shorter cables. They take up less space in the machine and not only that, they are quicker to install. The fewer number of connectors also saves time when connecting - which results in cost savings of 30 percent. Kollmorgen Salvagnini MachineThe other benefits of distributed servo technology are not inside the machine itself, - but in the control cabinet. Now that the drive’s heat loss no longer has to dissipate behind closed doors, the cost of cooling the cabinet is reduced. This produces two knock-on effects: firstly a smaller-scale and consequently cheaper cooling system and secondly, improved energy efficiency as a result of the control cabinet’s lower energy consumption. Savings of 30 percent have been estimated by Kollmorgen in real applications. Space-saving, increased energy efficiency and lower installation and assembly costs are three benefits of distributed servo technology embodied by the AKD-N servo amplifiers from Kollmorgen, which also bring tangible cost savings with them. It is interesting to note that this strict management of resources, in this case also incurs lower cost for the hardware. When considering the drive equipment part of the installation, a distributed architecture costs at least 3.5% less than the central control cabinet solution for the smallest Salvagnini machine. For systems with more performance and a greater number of axes, gains of up to 10 percent can be achieved.

Increased energy efficiency

Salvagnini are also using Kollmorgen's drive technology in another of their innovative advances. To replace the central hydraulic system, with a main pump and its correspondingly powerful asynchronous motor, they are using three highly efficient servo actuators, driven by Kollmorgen AKM servo motors and by S700 Series servo amplifiers, delivering power only at the moment the process requires it. Resulting from this, energy efficiency is increased, because the system drives only the active bending processes and does not have to keep the entire system with all its bells and whistles ready for operation. Thanks to the standard precision of the Kollmorgen drive axes, the required bending forces can be applied faster and with higher repeat precision, resulting in manufacturing quality improvement. All in all, Salvagnini has succeeded with the P2lean in developing both an economic, ecological and consequently highly competitive machine for panel bending companies. The distributed servo technology from Kollmorgen adds a valuable contribution to resource efficiency especially in terms of cabling, control cabinet space and cooling.

 

Kollmorgen Salvagnini Massari

Author: Fabio Massari, Salesmanager, Kollmorgen, Italy

About Kollmorgen
Kollmorgen is a leading provider of integrated automation and drive systems along with corresponding components for machine builders all over the world. With more than 70 years of Motion Control Design and application experience and profound knowledge of constructing standard and special solutions, Kollmorgen supplies solutions time and again that stand out in terms of performance, quality, reliability, and ease of use. As a result customers can achieve a market advantage which is beyond question.
For further information please contact us at [email protected]

 

Download as PDF

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Direct Drive Motors Improve Flexographic Printing Performance

Recent work done by Kollmorgen—a global leader in manufacturing motor and motion solutions—has shown that it is possible to synchronize components within the flexo printing process without mechanical transmission by using closed loop control technology. This synchronization is key to managing web tension throughout the process while ensuring a steady repeat length.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

How Cosmopack moved from specialized to flexible packaging solutions >

Learn how Cosmopack upgraded automated packaging line integration with decentralized motion architecture for more flexible packaging solutions.
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen Helps Salvagnini Build More Energy-Efficient Metal-Bending Machines >

Innovation, competency, service. Through 60 years in business, these three commitments have helped the Salvagnini Group achieve global leadership in the field of sheet-metal processing equipment. As the #1 worldwide supplier of panel benders, and one…

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >

The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…

Stop, hold and go safely: Motion tuning for vertical loads >

When designing motion for applications such as vertical gantries and hoists, you need to take special care to ensure operator safety and operational efficiency. Let’s discuss best practices for meeting the particular challenges involved.

What are the Five Major Components of a Brushless Servo Motor >

Servo motors are used in numerous markets to power machines, instruments, robots, and other factory automation applications. This blog addresses five major elements of a conventional brushless DC servo motor: the rotor, stator, bearings, feedback and…
What is a closed-loop system?

What is a Closed-Loop System? >

When learning about servo motors and servo systems, you’re likely to encounter the phrase “closed-loop system.” If you’ve ever wondered what that means and how it works, you’ve come to the right place. Let’s step through some of the most common…