Analog Position SetpointValid for S400, S600 The analog input can be used for the setting of the position from firmware version 3.10. The function is similar to a master/slave effect. |
Kollmorgen Support |
English | |
Speed adjustment with external position feedbackValid for S300, S400, S600, S700 |
Kollmorgen Support |
English | |
Memory CardValid for S700 |
Kollmorgen Support |
English | |
Reaction to fault situations S300-S700Valid for S300, S700 Depending on the current trouble, faults are managed differently (different error levels): |
Kollmorgen Support |
English | |
Setup of Acceleration Profile TablesValid for S300, S400, S600, S700 Create table with Excel, normalize current / position values |
Kollmorgen Support |
English | |
Analog Torque LoopValid for S400, S600 |
Kollmorgen Support |
English | |
Safe Reduced SpeedValid for S400, S600 |
Kollmorgen Support |
English | |
Motion Task SeriesValid for S300, S400, S600, S700 |
Kollmorgen Support |
English | |
Start of Motion Tasks in PROFIBUS operationValid for S300, S400, S600, S700 The Profibus protocol does not give any support for synchronizing the start of motion tasks. To start several drives synchronized, it can be useful to define the motion tasks by fieldbus but start them via a digital input. |
Kollmorgen Support |
English |
Don't know if you need a servo or stepper?
Motor Windings: Understanding How They Work and Affect Performance
Read MoreEngineer the Exceptional
Learn More