We are excited to introduce the launch of a brand new product selection tool – Kollmorgen Stepper Optimizer. Optimizer provides multiple ways for you to discover what Kollmorgen stepper motor works best in your application. Comprised in the tool are…
Horsepower (hp) is a measure of power, which can be further described as the rate at which work is performed. There are slightly different definitions for its conversion to the unit watts depending on the mechanism being described: mechanical,…
For many, “Made in Italy” is synonymous with Italian ceramic tiles, but did you know most tiles have been handled by “someone” other than Italian workers?
Europe's second largest dairy company, Arla Foods, has been using AGVs in their facilities since 2009. Read more to see how Arla Foods ensures everyone "gets milk."
Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications. In order to achieve the highest level of performance, the linear motor system must be commissioned…
Question: I need to operate a servo motor in a vacuum, what are some considerations?
Answer: In a word? Outgassing. You might think that proper motor sizing is a big issue, it always is, however if you can't conform to the other…
Most of the AKD drive’s parameters have a 32bit data size, but some parameters have a 64bit data size. Modbus communication on the AKD drive uses registers of a 16bit data size. So for a 64bit parameter, it takes four registers to send…
There is a lot of discussion about the 1.8 degree step angle versus 0.9 degree step angle of industrial hybrid stepper motors. Most stepper motors today have the standard step angle of 1.8 degrees, resulting in a 200 step per…
As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a…