Skip to main content
blog | What is horsepower and how is it utilized with servo motors |
|
2 minute read

Block and TackleBlock and Tackle Series Volume 1 - Horsepower

Welcome to our Block and Tackle series on Blog in Motion! We went back to basics to help answer some questions covering a variety of topics. We pose the question – and then offer an answer. We welcome your feedback on other questions or topics you might have – just add a comment to this blog post and we’ll add it to our list. Here we go!

Question: What is horsepower (hp) and how is it utilized with servo motors?
 
Answer:

Horsepower Horsepower (hp) is a measure of power, which can be further described as the rate at which work is performed. There are slightly different definitions for its conversion to the unit watts depending on the mechanism being described: mechanical, electric, boiler, metric, etc.. Our focus here will be on servo motor systems.

The SI unit Watt for the measure of power has been adopted by most countries of the world. However, the unit hp often survives because it is typically utilized to specifically define an electric motor’s output capability, reducing potential confusion between watts input, watts output [hp], and watts demanded by a load, while defining a system.

Just a side note – the watt (W) is named after a Scottish engineer, James Watt (1736-1819). (Also, remember to use the capital letter for units that are named after a person; like amp (A), volts (V), etc.

For electric motors: 1 hp = 746 Watts.
 
The basic equation for calculating horsepower is:

HPEnglish

The constant: 5252, is the rounded off calculation: 33,000 ft-lb/minute / 2π rad/revolution.

As the story goes, the standardized value of 33,000 ft-lb/minute was established in approximately 1783 by James Watt and Matthew Boulton based on the estimated output of a brewery horse

Since there are 1.35582 Nm/ ft-lb, the metric equivalent equation would be:
 
HPMetric

Horsepower (hp) defined by servo motor catalog data sheets is mostly used as a relative number for comparison purposes of continuous and/or peak capability when choosing a servo motor, since most applications require a knowledge of the required working torques and speeds.

Let us know if you have any questions on this or any other topic in motion!

Consult an Expert

AKME Series Servo Motors

AKME Series is built on the AKM platform and designed for use in Zone 2 and Zone 22 environments with ATEX and IECEx global certification.
Learn More

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Industrial printing press — a use case for Kollmorgen Essentials servo motors when upgrading from stepper motors

When should you convert from a stepper motor to a servo? >

Wondering when to convert from stepper to servo motors? Explore six signals, stepper limits, and how affordable servo motors simplify your motion control upgrade.
Automatic Pick and Place machine installing components on circuit board

How mechatronics design improves motion system performance >

Discover how mechatronics design boosts motion system performance by integrating servo systems and control for faster commissioning and integrated motion.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple

Choosing the Right Motor for HazLoc Machine Needs: Zone 2 and Zone 22 Made Simple >

Introducing Kollmorgen’s AKME servo motors—ATEX/IECEx certified and engineered for compact, versatile performance in hazardous environments where choices have been limited—until now.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.