Skip to main content
blog | Tips on How to Confidently Set Up Your Linear Motor System |
|
2 minute read

Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications. In order to achieve the highest level of performance, the linear motor system must be commissioned properly. This blog post addresses key areas to consider when setting up and commissioning a linear motor system. It is always important to refer to the installation and setup instructions provided by the manufacturer.

IC_Series_Ironcore_MEDIUM.jpg System wiring and cable management - Typically, a linear motor system consists of a stationary magnet "track" and a moving coil or "slider". This means you will have cables that are moving with the slider - so cable management is important. Major items to consider include cable flexibility, bend radius, and grounding and shielding practices. Wiring typically will consist of power leads, feedback, Hall-effect, and thermistors.

Initial Power-up - Once the motor is installed and wiring confirmed, begin the set-up process by making sure the drive's peak currents are reduced to safe levels, and place wooden blocks at each end of travel stop. A mis-wired linear motor could run away at high output forces, causing injury or even damage to the equipment.

Continuing on with the configuration, most servo drives have some method of setting up specific drive parameters associated with the specific motor you are driving. These parameters help set up how the motor will be commutated and configure the initial tuning loops. With the Kollmorgen AKD drive, most of the parameters are auto populated by selecting the correct motor model from a drop down list. In addition to the basic motor parameters, temperature sensing and feedback resolution also must be entered. It is very important to have the feedback resolution set correctly. In the AKD drive, resolution is defined by the magnet pitch divided by the encoder resolution.

Initial Testing - Encoder direction, motor phase sequence, and Hall sequence must match exactly for the system to both commutate properly, and the motor move as expected. The AKD drive has a means to test feedback resolution, as well as proper commutating direction within the Workbench environment.

Final Set-up - With the encoder and Halls properly aligned with motor phasing, and with the peak currents limited, a wake and shake process can be run to complete the commutation setup. Now you can carefully exercise the motor back and forth using short moves to be certain all is working as expected - and now your set-up is complete! You can continue to fine tune the system and optimize the performance on your machine.

Successful commissioning of a linear motor will ensure you are getting the most out of your system. You will be able to achieve the performance and precision you expect from a linear motor solution.

Consult an Expert

Direct Drive Linear Motors

Using Kollmorgen DDL direct drive linear motors, your machine can be simpler, faster, more precise and reliable. Pair your ironless, low profile or ironcore linear motor with an AKD or AKD2G servo drive for industry-leading power density.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights >

IC Ironcore DDL linear motors and AKD servo drives delivered 65% greater positioning accuracy and 15% higher productivity for this double-faced grinding machine.

Kollmorgen introduces new high-voltage IC Ironcore DDL direct drive linear motor >

Discover Kollmorgen’s new linear direct drive motor, engineered to move heavy loads with fast precision and to simplify machine design for the global marketplace.
Direct Drive Linear Technology Enables Large-Scale Production of Calcium-Titanium Ore Solar Cells

Direct Drive Linear Technology Enables Large-Scale Production of Calcium-Titanium Ore Solar Cells >

Learn how a major solar-cell manufacturer significantly increased productivity and quality using high-performance, zero-cogging IL Ironless DDL direct drive motors.
Incorporating a Direct Drive Linear Motor into Your High Performance Machine

Incorporating a Direct Drive Linear Motor into Your High Performance Machine >

When mechanical designers use conventional servo motors to drive ballscrews or rollerscrews for linear motion, they quickly encounter limits to the speed and precision they can attain. Direct drive linear motors provide substantially higher…
Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production >

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Cartridge DDR

Going Beyond Performance: Cost Savings with Direct-Drive Systems >

The performance benefits of direct-drive motors are well documented: industry-leading performance, improved accuracy, higher throughput, better reliability and quieter operations. This is because, unlike a conventional motion setup, a direct-drive…

Reducing Defects while Improving ROI in Metal Stamping with Direct-Drive Technology >

Compared to mechanical and hydraulic presses, mechanical servo metal stamping presses use high torque brushless motors to create more complicated stampings at faster speeds. But the type of motors used—a traditional geared or chain drive system or a…

Kollmorgen Is on the Perseverance Rover—And Extreme Environments Everywhere >

From the surface of Mars to the depths of the ocean, from the core of the earth to the core of the human body, Kollmorgen motion systems take on the most extreme environments.

How to Select a Direct Drive Linear Actuator >

There are several considerations when selecting a direct drive linear actuator for a specific application, such as the required speed, force, motion profile, available physical envelope, and environmental factors. This means the chosen actuator…