Skip to main content
blog | Meet a real pioneer in laser-guided AGVs |
|
2 minute read

Meet a real pioneer in laser-guided AGVs

In the mid-1970s, Tetra Pak started to use AGVs (automated guided vehicles) in their manufacturing and warehouse facilities. The purpose was to improve efficiency and safety when moving extremely heavy paper rolls from one place to another. Technical Product Manager Kenneth Palm at Kollmorgen has followed Tetra Pak’s AGV journey for more than forty years—including when laser navigation was introduced and changed the game.

Tough challenge

“A typical paper roll weighs a few tons and is difficult and dangerous to move,” says Mr. Palm. “The forklift drivers at Tetra Pak could hardly see what was happening in front of them as the rolls were so big, and driving speeds were not controlled.”
In 1976, Tetra Pak decided to install twenty AGVs in their plant in Lund, Sweden. Each AGV had a speed limit of 1 m/s and was guided via a wired floor network. The project was considered highly successful and Tetra Pak began to introduce AGVs in plants worldwide with the Lund factory serving as best practice.

The laser revolution

In the 1980s, laser technology took off in many industrial applications. “We were testing if laser could be used to navigate AGVs and the tests turned out well,” remembers Mr. Palm. “Tetra Pak had put their trust in our hands many times before, and in 1991 they decided to implement laser navigation in their Singapore factory.”
Big success, once again. Laser navigation made it easy to change the layout in the factory. Some adjustments in the software and laser reflector arrangement and you were up and running again. Tetra Pak started to upgrade many of their factories with laser navigation, and the next industry to follow was the Italian tile industry. Today Kollmorgen has an installed base of approximately 12,000 laser navigation vehicles.

Natural next step

The best thing would be, of course, if you could navigate with no reflectors at all. Now this is about to become reality through an NDC Concept called natural navigation. Watch this video to see the technology in action or contact us to find out more.
“The future of AGVs looks brighter than ever before,” concludes Mr. Palm. “AGVs are used in so many industries today, and with natural navigation coming up, the benefits will be even more obvious and valuable to customers.”

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…