Skip to main content
blog | Italian design brought to you by Kollmorgen |
|
2 minute read

Italian design brought to you by Kollmorgen

What comes to mind when you think about Italy? Certainly many of you will think about wine, pasta, Ferrari and Gucci. Others will think about architecture, music, textiles and other esthetically pleasing products. But few know that many things “Made in Italy” were at some stage handled by automated guided vehicles (AGVs).

Automation and automated guided vehicles (AGVs) have supported numerous Italian industries for decades, especially those working with large, heavy and/or hazardous materials and products. Moreover, Kollmorgen has been helping these industries improve their efficiency since the 1980s.

"Made in Italy"

One industry that realized early on the benefits of using AGVs in their processes was Italian Ceramics and Tile. In the 1980s, tiles had become, primarily, a mass manufactured, industrial product. Decorative styles had to adapt to the new production methods, which emphasized economies of scale.

To keep up demand, manufacturers introduced automation into their production, including AGVs for managing and storing raw and baked materials, and for handling pallets containing finished products. Many of these AGV installations were designed and developed by Kollmorgen partners in Italy.

Simplified logistics through automation

Designed to handle goods and products inside a plant, AGVs easily integrate with existing manual operations and other automated machines. AGVs move autonomously—automatically and without the need of an operator or fixed structures on the ground—guaranteeing a high degree of flexibility for future developments of a plant or warehouse. They can operate unrestricted in confined existing workplaces, leading to savings in time, energy and space requirements.

Increased safety in all environments

One of the greatest advantages of AGVs is workplace safety. Designed and programmed to execute their tasks without an operator, AGV movement is not hampered by visual limitations, common when handling large materials and products.

Built into all AGVs are components and routines that prevent collisions and accidents with human workers, workplaces fixtures and other AGVs.

Avoiding accidents helps maximize worker safety and reduce equipment maintenance/repair costs. Ultimately, AGV safety contributes to a harmonious workplace, increasing job satisfaction and product quality consistency.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…