Skip to main content
blog | Going Small - How Current Step Motor Technology Can Help You Reduce Machine Size |
|
2 minute read

Why So Small? WhysoSmall

As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a frame size of 1 3/16 inches, roughly the size of a modern day NEMA 11 motor. With a torque range of 1 - 12 oz-in, common applications at the time included printers, tape readers, and chart drive and display controls. Just like today, the small form factor of these motors allowed OEMs to reduce the overall size and footprint of their machines.

Achieving even smaller frame options means the stepper motor is now more versatile than ever. OEMs can better reduce the overall size and footprint of their machines, while maintaining maintenance-free, precise, and cost-effective motion control.

PMX Series Medium ImageFor example, small stepper motors used in chemical and blood analyzers allow OEMs in IVD and Life Sciences to further reduce the footprint of their products. The benefit? Smaller equipment can be kept on-site at local clinics and doctor's offices. Patients can be tested and receive medical diagnostics on-site, instead of making separate trips to the hospital.

The newly introduced PMX hybrid stepper series brings new NEMA 08, 11, and 14 frame sizes to Kollmorgen's stepper portfolio. Built with the same hybrid construction as their larger counterparts, these smaller motors offer a torque dense solution in a much smaller form factor.

More information about this new step motor line is available here.

Consult an Expert

PMX Series

The PMX family of hybrid stepper motors offers unmatched versatility through a wide range of standard and customizable options, unmatched value through exceptional performance at an affordable cost, and unmatched reliability through Kollmorgen’s superior motion expertise and build quality.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

5 Mistakes to Avoid When Specifying a Stepper System

5 Mistakes to Avoid When Specifying a Stepper System  >

Stepper systems can be efficient, powerful and quiet — but only if you get it right. When specifying stepper motors and drives, here are 5 common mistakes to avoid and 5 best practices to implement, speeding your development of a successful machine.

Kollmorgen Stepper Motor Selection Guide >

Kollmorgen’s stepper motors are designed with versatility, ease–of–use, and cost-effectiveness in mind. They provide high torque in a small package and come in a wide range of standard sizes, constructions, windings and options.

Get Exact Positioning Without the Complexity with Stepper Motors >

If you’re looking for precise motion with easy setup, then stepper motors should be your first choice when building or upgrading a machine.
What You Need to Know When Selecting a Drive for Your Stepper Motor

What You Need to Know When Selecting a Drive for Your Stepper Motor >

To get the most out of your stepper motor, you need to pair it with the proper drive. There are three critical elements to keep in mind when making your selection: voltage, current and inductance. Each one plays an important part in a motor’s…

Why Does My Stepper Motor Get Hot? >

All electric motors heat up during operation, which is simply a product of passing current through a coil of wire. Electric motors use copper wire to form coils that are part of the electromagnetic circuit required to produce rotation. While copper…
Diagnostic Imaging: Motion for Every Modality

Diagnostic Imaging: Motion for Every Modality >

An aging population, a growing burden of disease, continuous development of new clinical applications, and global advancements in the standards of disease prevention, early detection, diagnosis and treatment. For all these reasons and more,…
Servo vs Stepper

Stepper Motor or Servo Motor: Which Should it be? >

This article presents an overview comparison of stepper motor and servo motor capabilities to serve as selection criteria between the two technologies.

The Big Debate – Stepper vs Servo >

What is the best motor technology to use in a motion control application? There are numerous technologies to create motion, from hydraulic to pneumatic or electromechanical. In the world of precision motion control, many machine designers face a…
Kollmorgen stepper motor

How to Select a Stepper Motor >

Knowing how to selct a stepper motor is critical for optimal performance. Use our speedy, dependable Stepper Optimizer tool for precise selection.