Skip to main content
blog | AGVs in the new industrial landscape |
|
2 minute read

AGVs in the new industrial landscape

There is a shift going on in manufacturing industries and warehouses. The demand for automation, for example with Automated Guided Vehicles (AGVs), is growing but also the demand for a new type of workforce who can help realize the power of automation.

New truths

In a recent study, management consultancy firm Boston Consulting Group shows the effects Industry 4.0 will have on the workforce. Self-driving logistics vehicles, or AGVs, are one of ten selected foundational technologies driven by an overall need for automation to reduce costs and enhance productivity and growth.

One conclusion in the study is that the total amount of jobs will increase despite the increased level of automation. In Germany, the country chosen for the study, the most likely scenario is that 350,000 new jobs will be created in the manufacturing industry by 2025. This is a very different scenario from what has happened in the past. Between 1997 and 2013, automation and offshoring caused an 18 percent decrease in the workforce while production volumes increased.

Start with AGVs

The study also concludes that working roles will change. In short, machines will take care of routine-based work while skilled operators will make sure all the machines are performing at their very best. Some possible future roles are industrial data scientists and robot coordinators.

However, change takes time and should never be underestimated. Which is why AGVs are a good way to kick-start your own fourth industrial revolution. For years, AGVs have been used to assist staff in manufacturing industries and warehouses. As the technology is proven and the level of automation relatively is easy to understand, most people can continue to take on new roles and feel comfortable with that.

You can find more valuable insights in our previous article on Industry 4.0 and AGVs.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…