Skip to main content
blog | What is what in the driverless world? |
|
2 minute read

Rapid development in the industry makes this a hard question to answer. Join us for a ride in a world full of acronyms and expressions.

New vehicles, new names

The acronym AGV, short for automated guided vehicles, has been used for decades. However, in the last fifteen years, there has been an explosion of new types of driverless vehicles for the industrial and logistics sectors. You still find many AGVs out there, but also carts, mobile robots and automated lift trucks.

Having said that, the similarities are greater than the differences. No driver, central control and the ability to send and receive information are still characteristic features of automated guided vehicles.

Examples of definitions

Let’s take a look at some of the most common acronyms and expressions in the world of automated guided vehicles.

Acronyms

What is what in the driverless worldAGV – Automated (or Automatic) Guided Vehicle. A driverless vehicle for predictable travel routes and efficient movements of items in manufacturing and logistics. Based on a customized or standardized (e.g., lift truck) vehicle platform.

AGVS – Automated Guided Vehicle System. A system with a number of AGVs.

AGC – Automated Guided Cart or just Cart. A vehicle with basic functionality (carry or draw loads) and simple navigation (magnetic tape).

LGV – Laser Guided Vehicle. AGV guided by laser technology. Kollmorgen (NDC) was the inventor of laser-guided vehicles in the early 1990s.

AMR – Autonomous Mobile Robot. Driverless vehicle equipped with autonomous controller allowing the vehicle to take any travel route. The vehicles are easy to install and suitable where service is more important than productivity.

Expressions

Automated lift truck. An automated guided vehicle based on a standardized lift truck.

Driverless vehicle/Self-driving vehicle. All vehicles that can be run without workforce in industries and warehouses. The automotive industry uses the same expression for cars that can drive themselves.

Mobile robots. Think about your robot vacuum cleaner in your home, and you have the idea for a mobile robot. A vehicle with no need for a fixed navigation system.

Conclusion

There are many ways to describe automated guided vehicles, but the fundamental principle remains the same: Efficient and safe movements of materials and goods from A to B.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…