Skip to main content
blog | The basics of automated guided vehicles |
|
2 minute read

Automated guided vehicles (AGVs) are designed to move materials in factories and goods in warehouses. They are more friendly than manually operated vehicles and more flexible than fixed automation solutions such as conveyor belts.

Works almost everywhere

The basics of AGVAutomated guided vehicles come in many sizes and degrees of customization. Some are based on purpose-built platforms while others are based on standard lift trucks. There is also an increasing number of compact, fast-moving vehicles designed for general purposes like carts and mobile robots.

You find automated guided vehicles in a wide variety of industries, including automotive, ceramics and tiles, distribution, electronics, food and beverage, paper and printing, and steel and heavy goods. Hospitals represent another area where these vehicles bring value by performing repetitive tasks, thereby releasing time for staff to take care of the patients. What is more, automated guided vehicles are especially beneficial in labor-intensive, hazardous or environmentally sensitive conditions.

Controlled driving

There are two ways to guide an automated vehicle: Via physical paths on the floor (magnetic tape, inductive wire, paint) and via free-ranging items (laser reflectors, natural objects in the environment). Every vehicle has corresponding sensors, allowing it to follow a specific path. The path is controlled by computer software for the vehicle fleet which, in turn, is integrated into the plant’s warehouse management and business enterprise systems.

The precise control of automated guided vehicles helps boost efficiency, safety and quality in factories and warehouses. Working repetitively also leads to predictability – you get the chance to improve your processes and reduce quality issues to a minimum. Well-defined safety zones further reduce the risk of damage to goods, pallets and racks. Above all, controlled driving minimizes the risk of employees getting injured.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…