Skip to main content
blog | Staying on top all the time |
|
2 minute read

Staying on top all the time

Your Automated Guided Vehicles (AGVs) are up and running. Your staff understands and embraces the change to the new way of working. Now you need to secure long-term success with good management of service and upgrades. A job that is easier than you might think. 

The early changes

A typical AGV project includes going through the current process flows, defining smart driveways and explaining to people why AGVs are needed and how they work. Usually, performance measurements show efficiency improvements after only a few months. The next step is to fine-tune the new process flows to perfection.

“In most AGV projects, we make changes to the system during the first one to two years because the client sees what could be optimized,” says Jürgen Kammer, APM-specialist at Jungheinrich. “Changing the logic is quite easy with open and scalable systems such as NDC8 from Kollmorgen.”

AGVs are often installed in existing manufacturing plants and warehouses, with little or no interruption of daily work. Changing the system goes just as smoothly.

Easy to maintain

Your AGVs, for example, automated lift trucks or mobile robots, need service at regular intervals. Software upgrades are often related to ERP or WMS upgrades.

“You want your AGV system to perform all duties with the same level of quality over time,” says Peter Ekelund, Director Services at Kollmorgen. “Just make sure you service your trucks and robots in time and upgrade software only when necessary.”

The controlled driving of AGVs also contributes to lower service costs, as an automatically driven vehicle has much less wear and tear compared to a manual lift truck.

Preparation is the key to success

This is the third article about AGV installations. The first dealt with the importance of change management; the second described installation and integration work and here we focus on service and upgrades. The key takeaways this time are:

  • Allow easy changes to the software – choose an open platform
  • Upgrade without shutdowns – pick the right software and timing
  • Expect lower service costs – AGVs are careful drivers

Kollmorgen has been a driving force within vehicle automation for decades. With an installed base of 20,000 vehicles, we have seen and solved almost any challenge there is to AGV installations. Benefit from our knowledge by subscribing to our newsletter and contact any of our partners to get started with your AGV installation.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…