Skip to main content
blog | Making AGVs thrive in your plant |
|
2 minute read

Making AGVs thrive in your plant

Installation and integration of AGVs (Automated Guided Vehicles) in manufacturing plants and warehouses is about organizing a strong project team and defining smart driveways. Challenging existing ways of working is part of the process and often a valuable source of insight and inspiration for making further improvements in your plant. 

True teamwork

A typical AGV project consists of people from production, IT and management. To succeed you need to understand the workflows, the digital infrastructure and the business case.

“It is much easier to install and integrate AGV systems than most people think,” says Jürgen Kammer, APM-specialist at Jungheinrich. “Sure, AGVs are automated machines, but the system is relatively small with no need for gigabytes of database space. Start by creating an internal team to make sure the project gets the right attention.”

The most important team member is the one who will be responsible for the AGVs in the long run. This person is often the production or warehouse manager.

Driveway design

Every project involves going through the current process flows. Where and how will the AGVs pick up and leave the loads?

“AGVs drive in a disciplined manner and thereby reduce waste and the risk of accidents,” says Peter Ekelund, Director Services at Kollmorgen. “You have to spend some time on figuring out the smartest driveways, but this is a good exercise. A typical customer reaction is that ‘we should have done this many years ago’ when the efficiency gains of a more structured workflow become apparent.”

Simulations are recommended when preparing for the new AGV system. You can often install most parts while your production up and running, and with some planning you can do the rest during weekends and vacations. Change management is key to ensuring that the staff feels comfortable with the new way of working, particularly if manual trucks are still used in some areas.

System connection

The AGV system needs to get data from and give data to other systems such as ERP, WMS and voice systems. AGVs based on an open platform simplify system integration as well as future changes and upgrades.

“Sometimes you have to upgrade existing systems due to the new AGV system but this is something you have to do anyway sooner or later,” says Per Hansson. “With AGVs, you get better and more precise input to your existing system infrastructure, important to consider when calculating the return on AGV-related investments.”

The digitalization of the industry is based on collecting, analyzing and using big amounts of structured data. AGVs can contribute to your future vision.

Wrapping it all up

Time to summarize. Here are the key takeaways for installing and integrating AGVs:

  • Start an internal project – involve production, IT and management
  • Define required system performance – draw up the best driveways
  • Clarify who will be in charge of the AGV system (key team member)
  • Use the improved data flow to strengthen your business

The next article will deal with service and support of AGV systems. Sign up for our newsletter to make sure you get it. And as always, feel free to contact any of our partners.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…