Pular para o conteúdo principal

Search Articles

FPGA Based Sin Cos Encoder Processing inglês
Tuning - Built-in Frequency AnalysisValid for S300, S700 inglês
Expansion Card FANThe option FAN Option (S700: F2, S600:FAN) is an electronics, which controls the velocity of the integrated fan depending on temperature measurement. This reduces the overall noise emission of the servo amplifier. inglês
Understanding Kollmorgen Stepper Motor Current UnitsThe stepper motors' continuous current rating in the Kollmorgen documentation is in units of dc current.  This is based on the actual DC current that the motor can handle, and applies to older drives using full step or half step resolution.  Most stepper drives s inglês
Manual - KAS 2 Axis Demo / TrainerAttached is the : - Getting Started Sheet - Demo Manual for the KAS 2 axis demo trainer. inglês
AKD Series Drive Connections for the Goldline Series MotorsThis article describes Goldline motors resolver feedback connections, Goldline motor power connections, AKD resolver feedback parameter values, and AKD Motor.Phase values. inglês
AKD Homing to Marker on Secondary Feedback (X9) inglês
Calculating Actual Motor Torque and Current with PN Motion Engine ECAT  (Ethercat) Object 6077 is part of the standard ECAT PDO mappings to KAS from the AKD drive. From the PDO section tab of an AKD axis in an an IDE project. inglês
Motor Phase Wiring - S300 or S700 to KBM Preferred StandardThe preferred standard electrical connections between the S300/S700-drive to KBM(s) - frameless motor, unless specifically stated otherwise, are based upon a C.C.W. rotation of the rotor as viewed from the lead-exit end of the motor, for a positive count direction of the position-loop. Hence the… inglês