Pular para o conteúdo principal

Search Articles

S300 Safety Characteristic Data Device EN 13849-1 EN 61800-5-2 PFHD (1/h) TM (Years) inglês
S600 Safety Characteristic DataThere is no certification for the S601-620 drives according to EN 13849-1 or EN 62061. inglês
S748-772 Safety Characteristic DataThis is valid for drives with HWR >= 02.10. Device S748-772 Operation mode EN 13849-1 EN 62061 PFHD (1/h) TM (Years)  STO1/2-Enable single channel PLd, Cat.3 SIL CL2 7.05E-08 20 STO1-Enable+STO2-Enable dual… inglês
AKD DC Bus LinkThe DC bus link, or connections, of the AKD drive can be used to connect the DC bus of one drive to the DC bus of another drive.  The connection is done in parallel between two or more drives, with the maximum number of drives being limited by the total sum of the current ratings, as specifi inglês
KAS HMI, obsoleteThis article provides information on obsolete KAS HMI panels. inglês
AKD Control Loop Update Rates Digital current controller (670 ns) Digital speed controller  (62,5 µs) Digital position controller (250 µs) inglês
AKD MODBUS.MSGLOG and MODBUS.MSGDUMPMODBUS.MSGLOG and MODBUS.MSGDUMP When MODBUS.MSGLOG is set to 1 it enables the logging of the raw Modbus data received by the drive via the report given by MODBUS.MSGDUMP. inglês
AKD EtherNet/IP Cyclic I/O Assembly and Explicit MessagingIn this application note, we’ll demonstrate the different command types supported by the AKD EtherNet/IP drive. inglês
AKD EtherNet/IP In Position Window StatusAKD EtherNet/IP “In Position Status”. inglês