DRIVE-CLiQDRIVE-CLiQ ist eine offene Geberschnittstelle. Kollmorgen bietet AKM Motoren mit Singleturn oder Multiturn Drehgeber und DRIVE-CLiQ-Schnittstelle an. Das Motorfeedback kann über einen M12 Stecker an das Antriebssystem SINAMICS angeschlossen werden.
alemão
BiSSDie bidirektionale digitale Sensor- Schnittstelle BiSS sichert die Kommunikation zwischen Positionsgeber und Messgerät bzw. Antriebssteuerung und überträgt bei Bedarf gleichzeitig Messwerte von bis zu 8 Sensoren.
Cogging CompensationThe AKD supports similiar to the Servostar line a cogging compensation/suppression functionality, which can be used to increase the synchronism of the motor movement.
A detailed description how to use this functionality can be found in the workbench help:
inglês
KAS Web Server - Overview The KAS PxMM Controllers contain a built in webserver for access to the PxMM without having to work through the IDE. Functionality include:
inglês
Endat 2.2: Inter-compatibility with various encoder typesIn October 2016, an inter-compatibility test was performed together with the company Heidenhain. In this event, the AKD was tested successfully with various types of Heidenhain Endat 2.2 encoders.
The devices tested can be found in this article.
inglês
AKD DS402 Position Scaling SetupSome History: We have been making EtherCAT drives since ~1998. That was before EtherCAT.org and before the EtherCAT standard. We don’t want to “break” our existing Customers' applications so we kept the same original scaling in the AKD.
inglês
PLCopen Axis ConfigurationThis article features a video showing the steps to create a new PLCopen axis in the KAS IDE.