AKD Backup FPGA Notice
This notice is to inform AKD owners about a bug in the Backup FPGA firmware. This page provides information that will help you understand and update the backup FPGA firmware to the latest version.
Notice
What is the bug?
During recent internal development activities, it was discovered that a specific sequence of events could lead to an unintentional motor holding brake release due to corrupted firmware.
The condition may occur from the following sequence of events:
- Initiate a user firmware file download (via Workbench or Fieldbus)
- Interrupt the download process (for example by disconnecting the Ethernet cable)
- The firmware may be corrupted due to the interruption
- Power cycle the AKD (remove power, re-apply power)
- If the firmware was corrupted, the AKD will power up using the Backup FPGA firmware
If items 1-5 occur, the Motor Brake will unexpectedly disengage. The reason for this behavior is an issue in the Backup FPGA firmware.
What is the “Backup FPGA firmware”?
The Backup FPGA is programmed at factory and is not a part of the user firmware file. The Backup FPGA image is not normally loaded or used. Updating the user firmware does not touch the Backup FPGA firmware and vice versa. The Backup FPGA’s purpose is to provide a fallback mechanism to download firmware when the user firmware is corrupted. This Backup FPGA firmware supports only the minimal functionality necessary to communicate so the user can flash the AKD with a new user firmware.
What are the effects of the bug?
If the AKD must boot up with the Backup FPGA firmware due to corrupted user firmware, it is possible the AKD will energize the holding brake with 24 Volts, causing the brake to disengage (if there are no additional switches such as a safe brake relay).
If you have a gravity-sensitive load that is not properly secured, the load could begin to move uncontrollably, simply due to the kinetic energy of the load.
Is my AKD affected by the bug?
The following model numbers are affected by the bug:
- AKD-P; AKD-B; AKD-T; AKD-M
- KC1-B; KC1-M
NOT affected are models beginning with AKD-N, AKD-C
The following serial numbers are affected by the bug:
- B-0901-00001 – B-1714-00255 (“-00256” and higher have the updated firmware included)
- P-0901-00001 – P-1715-00004 (“-00004” and higher have the updated firmware included)
- R-0901-00001 – R-1714-00221 (“-00222” and higher have the updated firmware included)
- T-0901-00001 – T-1715-00000 (“-00001” and higher have the updated firmware included)
Is my application affected by the bug?
If you are using the affected AKDs listed above, your application may or may not be affected by this bug. Please follow this flowchart to check if this bug affects your application:

How do I fix it?
If your application is affected, there are several ways to mitigate risk without upgrading your firmware. Each countermeasure alone should eliminate the risk:
- Secure the load or move to a safe position before updating the standard AKD firmware.
By securing the load or moving to a safe position, disengaging the brake after a failed firmware update attempt will have no effect. This is required by regulatory agencies, so you are likely doing this. - Unplug the motor when updating the standard AKD firmware.
By unplugging the motor from the AKD the brake is also disconnected. Hence it will always stay engaged - Update the Backup FPGA firmware.
We recommend that you update the Backup FPGA firmware if you cannot apply either of the above-recommended countermeasures.
Please contact your Kollmorgen Application Engineer if you have any questions this notice or KDN does not answer.
Instructions
The following steps may be taken to update the Backup FPGA on AKDs.
- Connect to your drive with Workbench.
- Select the terminal and type DRV.INFO then execute the command.

In this example the Backup FPGA version can be identified by looking for the "FPGA" section and "Resident image" alias Backup FPGA.
The coding for the backup FPGA version is as follows: “FPB00x_yyyy_yy_yy”, where “x” represents a certain FPGA type and “y” represents the version number. The upper number represents the most significant version number. All versions lower than “0602.00.01” are affected.
In this example the version is “0300.00.00” , which is a backup FPGA version with the brake issue. - Go to the main window and click on Update.

- Choose the correct Backup FPGA to download, which matches your drive type. Note see Backup_FPGA_v0602_00_01.zip. Click Open
- Workbench filters the correct type matching your drive type.
In this example the drive type is AKD-P-00307-NBCC-0000, where the bold characters need to match the file name. Workbench filters the correct file to be AKD-P-NBCC-V0602-00-01-R-FPGA.i00.

- Wait until Workbench has finished the download procedure.

- Verify that the upgrade of the Backup FPGA was successful by repeating steps 2 and 3. Check that the version is 0602_00_01. If the version matches, the brake issue in the Backup FPGA is resolved.
FPGA Version : FP0006_0602_00_00 Operational image : FP0006_0602_00_00 Resident image : FPB006_0602_00_01 Size : 45
FAQ
Frequently Asked Questions
Probably not. If you are an end user with an AKD working just fine in the field, we suggest you leave it alone.
If you are an OEM, and you think you might want access to the latest features, then you may want the latest (operational) firmware and Workbench. If you do decide to update the (operational) firmware and corresponding Workbench, please update your Backup FPGA firmware first. Make sure the drive accepted the updates and has the latest Backup FPGA firmware. Then, if you wish to proceed with updating the (operational) firmware and corresponding WorkBench, feel free to do so.
All of the necessary files are on KDN.
During recent internal development activities, it was discovered that a specific sequence of events could lead to an unintentional motor holding brake release due to corrupted firmware.
The condition may occur from the following sequence of events:
- Initiate a user firmware file download (via Workbench or Fieldbus)
- Interrupt the download process (for example by disconnecting the Ethernet cable)
- The firmware may be corrupted due to the interruption
- Power cycle the AKD (remove power, re-apply power)
- If the firmware was corrupted, the AKD will power up using the Backup FPGA firmware
If items 1-5 occur, the Motor Brake will unexpectedly disengage. The reason for this behavior is an issue in the Backup FPGA firmware.
The following flowchart will guide you to help determine whether you are affected by the Backup FPGA firmware. If you are, please download the new files and instructions.

The sequence of events leading to possible brake disengagement is described in this flow chart. The box marked in red shows the wrong behavior due the fault condition.

No. The Backup FPGA firmware is not part of the standard beta or production release of operational firmware. The Backup FPGA firmware is programmed separately, and requires special files and process. The files and process are listed in this article.
No. The Backup FPGA firmware is not part of the main AKD firmware and is not used under normal operating conditions.
Connect to the AKD. Go to terminal view. Enter the command “DRV.INFO”. In the section "FPGA", you can read the Backup FPGA firmware version.
For example:
FPGA Version : FP0006_0602_00_00 Operational image : FP0006_0602_00_00 Resident image : FPB006_0602_00_01 Size : 45
The version for the Backup FPGA firmware can be found under "Resident image".
The coding is a follows: FPB00x_yyyy_yy_yy, where “x” represents a certain type, and “y” represents the version number. In this example the version is 0602_00_01.
All Backup FPGA firmware versions FPB0xx_0300_00_00 through FPB0xx_0602_00_01.
0300_00_00 was released in March 2012; 0602_00_01 was released 10 April 2017.
The next question, How can I figure out the current version of my Backup FPGA firmware?, explains how to discover what version you have.
Yes, you can update the Backup FPGA firmware yourself. Instructions to upgrade the Backup FPGA firmware can be found on this page or downloaded. The downloadable file may also be found as an attachment at the bottom of this page.
No. The brake will not disengage during a firmware download.
The brake may disengage during a reboot if the download fails and the user firmware has been corrupted.
The following serial numbers are affected by the bug:
- B-0901-00001 – B-1714-00255
- P-0901-00001 – P-1715-00004
- R-0901-00001 – R-1714-00221
- T-0901-00001 – T-1715-00000
The following model numbers are affected by the bug:
- AKD-P; AKD-B; AKD-T; AKD-M
- KC1-B; KC1-M
NOT affected are models beginning with AKD-N, AKD-C.
One of the following countermeasures can prevent this issue:
- Secure the load during firmware download
- Remove the motor connector from the AKD before starting firmware download (remove power from the AKD before disconnecting any cables!)
- Upgrade the Backup FPGA firmware on the AKD to version FPB0xx_0602_00_01 or higher.
Contact Information
For application-engineering assistance:
North America: +1-540-633-3545
South America: +55-11-4191-4771
Italy: +39-0362-594260
Turkey: +90-212-282-75-80
Rest of Europe: +49 (0) 2102-9394 0
India: +91-22-6188-0200
Japan: +86-400-661-2802
Mainland China: +86-400-661-2802
Hong Kong, Taiwan R.O.C. and Southeast Asia: +852-2503-6565
Ask a Question
Have more questions? Ask the community.
Back to top
Home >
Knowledge Base >
FAQs >
Downloads >