What is the Backup FPGA Bug?
During recent internal development activities, it was discovered that a specific sequence of events could lead to an unintentional motor holding brake release due to corrupted firmware.
The condition may occur from the following sequence of events:
- Initiate a user firmware file download (via Workbench or Fieldbus)
- Interrupt the download process (for example by disconnecting the Ethernet cable)
- The firmware may be corrupted due to the interruption
- Power cycle the AKD (remove power, re-apply power)
- If the firmware was corrupted, the AKD will power up using the Backup FPGA firmware
If items 1-5 occur, the Motor Brake will unexpectedly disengage. The reason for this behavior is an issue in the Backup FPGA firmware.
Home >
Knowledge Base >
FAQs >
Downloads >