Skip to main content
Success Story | 2 minute read

Compact, Efficient Motion Powers a Submersible Robot for In-Service Inspection of Fuel Storage Tanks

Founded in 2016, Square Robot is an innovator in robotic inspection of above-ground tanks used to store diesel fuel, gasoline, kerosene, various oils and other products. Through ongoing development of robotic, dataacquisition and data-processing technologies, Square Robot is uniquely positioned to enable in-service inspections for ensuring tank integrity and safety.

“The integration of a frameless motor into Square Robot’s propulsion system was an incredible achievement for the team. We’ve been researching and developing technology to address the challenges that gasoline and other low-flashpoint materials bring, so it was great to collaborate with Kollmorgen and leverage their motor expertise during this successful SR-3 project.” — Charles O’Connell, Director of Mechanical Engineering, Square Robot

Challenge

Eight thrusters are required to give the submersible robot six degrees of freedom in navigation. When a commercially available thruster proved to be incompatible with gasoline and other petrochemicals due to the materials used, Square Robot’s engineering team turned to a market leader trusted for its expertise in specialized motion applications: Kollmorgen.

The challenge was to design a submersible robot compact enough to fit into tight entryways originally designed to accommodate a single human, maneuverable enough to closely inspect the entire tank while avoiding columns and other obstructions, versatile enough to perform in fluids of widely varying weight and viscosity, and efficient enough to complete inspections lasting eight hours or more on a single battery charge.

Solution

Eight thrusters are required to give the submersible robot six degrees of freedom in navigation. When a commercially available thruster proved to be incompatible with gasoline and other petrochemicals due to the materials used, Square Robot’s engineering team turned to a market leader trusted for its expertise in specialized motion applications: Kollmorgen.

A compact KBM frameless servo motor, housed in a nitrogen-filled pressure vessel with a dynamic seal, was selected to power the thrusters on Square Robot’s next-generation SR-3 submersible. Kollmorgen modified the KBM windings to meet the application’s exact performance requirements — including the ability to maintain relatively high torque at high rotational speeds. Kollmorgen’s Frameless Motor Performance Curve Generator provided essential data for achieving the optimum winding design.

The pressure vessel isolates the KBM motor windings to prevent ferrous sediment buildup, unlike the previous design that bathed the encapsulated windings directly in the tank fluid. The KBM motor also incorporates integrated Hall sensors that allow thrusters to achieve velocity as low as zero when necessary.

Image 1

Results

Highly modified, compact KBM motors deliver efficient thruster performance even in challenging lower-density and higher-viscosity fluids. Hall sensor feedback enables a full velocity range for total navigational control, even allowing the bottom scanner to be precisely positioned within ½ inch of the tank shell. The ruggedized design ensures reliability in challenging in-tank environments.

Working in concert with Square Robot’s preferred drive, the motion system delivers efficient performance across the full range of speed/ torque demands, maximizing the robot’s battery life so that it can complete inspections lasting eight hours or more on a single charge.

Yet despite all the modifications, this custom level of performance is achieved using the commercial-off-the-shelf KBM servo motor platform — ensuring that Square Robot can count on long-term manufacturability, availability and affordability.

Image 2

About Kollmorgen

Kollmorgen, a Regal Rexnord Brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, linear actuators, AGV control solutions and automation platforms. We deliver breakthrough solutions that are unmatched in performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Download as PDF

Exoskeleton

From the promise of greater freedom and mobility among aging populations to empowering human performance in industrial applications, the demand for exoskeletons is significantly rising. But effectively emulating human movement, safely, is a challenge.
Learn More

Exoskeletons at Scale: Accelerating the Transition from R&D to Full-rate Production

The exoskeleton market is still in its infancy — but evolving quickly and ripe with opportunity. It’s a double-edged sword for OEMs who must identify the most impactful applications and crack the code on full-scale production, which presents a new set of challenges and considerations.

Projects that seemed feasible during R&D and even LRIP can quickly become impossible at scale for a variety of reasons. So how can OEMs foresee (and avoid) issues that may arise as they ramp up production? Here, we’ll cover key tips and insights.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…