Skip to main content

All Together For Innovation: More perspectives mean better ideas and better products >

At Kollmorgen, there are more and more female employees every year, which really helps to broaden overall perspectives. Everyone agrees that diversity drives innovation and these values apply to the group at every level.

Interoperability: What it is, and why it matters in the age of automation >

We are now living in a digital world. E-commerce consumers expect goods to be delivered faster and more flexibly than was the case just a couple of years ago. Organizations, retailers, and their warehouse service providers therefore need to find new…

What is a Closed-Loop System? >

When learning about servo motors and servo systems, you’re likely to encounter the phrase “closed-loop system.” If you’ve ever wondered what that means and how it works, you’ve come to the right place. Let’s step through some of the most common…

Motors for Robotics: Do You Really Need to Compromise?  >

Robotic joint design almost always involves tradeoffs. But does it have to be that way? Let’s look at the three most common compromises.

Get Exact Positioning Without the Complexity with Stepper Motors >

If you’re looking for precise motion with easy setup, then stepper motors should be your first choice when building or upgrading a machine.

What is the Difference Between a Servo Drive and a Motion Controller? >

In many applications, both a motion controller and a servo drive are required to complete the system. But what is the difference between a motion controller and a servo drive?

What You Need to Know When Selecting a Drive for Your Stepper Motor >

To get the most out of your stepper motor, you need to pair it with the proper drive. There are three critical elements to keep in mind when making your selection: voltage, current and inductance. Each one plays an important part in a motor’s…

Overcoming the Limitations of Missile Design >

Missiles operate in some of the most demanding conditions. They can experience massive heat flux when going through the layers of the earth’s atmosphere and because of the sheer speed that the missile is traveling at. With speeds in excess of 10,000…

The Right Supplier Partnerships Can Mitigate Risk in Defense Programs  >

For rapidly evolving Aerospace and Defense (A&D) requirements, engineers are facing many challenges to keep up with ever evolving demands. From supply chain issues to changing government regulations, companies are being tasked with not only…

What is Considered a Low Voltage Motor? >

The Low Voltage Directive defines low voltage from 50 – 1000 Vac, or 120 – 1500 Vdc, which is based on the mains voltage used to power the electrical system and ties in with specific IEC regulations on safety and risk of shock and arcing. When low…

Automation in a Single Day with Game-Changing DIY Platform >

Accessible and affordable automation for all has made a giant leap forward with the release of an AMR platform that enables users to install out-of-the box automation technology in less than a day.

Why Does My Stepper Motor Get Hot? >

All electric motors heat up during operation, which is simply a product of passing current through a coil of wire. Electric motors use copper wire to form coils that are part of the electromagnetic circuit required to produce rotation. While copper…