Skip to main content
blog | Why Does My Stepper Motor Get Hot? |
|
2 minute read

All electric motors heat up during operation, which is simply a product of passing current through a coil of wire. Electric motors use copper wire to form coils that are part of the electromagnetic circuit required to produce rotation. While copper is a very good conductor, it does have resistance that causes the copper to heat up. The amount of current delivered to the motor along with the winding resistance determines how hot it gets. The nature of stepper motor operation requires full rated current to be applied at all times, which differs from a servo motor that provides only the required current to produce the desired motion.

Stepper motor heat sources

Stepper motors are designed to accommodate the heat generated when operated at their rated power. While the majority of the generated heat comes from the motor windings, there are other sources of generated heat in hybrid stepper motor designs, such as vibration and eddy currents. Since the motor is driven by a series of square wave pulses filled with various harmonic frequencies, the motor will vibrate. This vibration not only contributes to audible noise, but additional heat as well. Eddy currents are another heat producing source. The lamination steel used in the stepper motor stator can generate recirculating currents (Eddy currents) that tend to add more heat to the stator. All the heat that resides in the stepper motor stator transmits to the motor housing and endbells, which creates a motor that is definitely hot to the touch.

How to reduce stepper motor heat

While it is natural for a stepper motor to run hot, there are ways to reduce the heat. The common method is to utilize a stepper drive feature called idle current reduction that reduces the current applied to the motor to a set percentage when the motor is not moving. In many cases, the full holding torque of the stepper motor is not required during idling conditions, so the applied current can be reduced, which in turn reduces the heat generated by the motor. Other more sophisticated methods to reduce heating is to shape the current wave to minimize unwanted harmonics and to smooth out the pulses delivered to the motor, or to use a drive’s microstepping feature. Heat sinking methods can draw away heat from the motor to allow it to operate cooler as well.

It is also possible that a stepper motor and drive are mismatched, meaning that the drive’s output current is higher than the motor’s rated current. Most stepper drives can adjust the output current setting using either dip switches on the drive or within the drive software.

Kollmorgen offers online design tools that help calculate the expected motor temperature to determine if the motor and drive are optimized to prevent over heating in the motor based on the application requirements.

Consult an Expert

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

5 Mistakes to Avoid When Specifying a Stepper System

5 Mistakes to Avoid When Specifying a Stepper System  >

Stepper systems can be efficient, powerful and quiet — but only if you get it right. When specifying stepper motors and drives, here are 5 common mistakes to avoid and 5 best practices to implement, speeding your development of a successful machine.

Get Exact Positioning Without the Complexity with Stepper Motors >

If you’re looking for precise motion with easy setup, then stepper motors should be your first choice when building or upgrading a machine.
What You Need to Know When Selecting a Drive for Your Stepper Motor

What You Need to Know When Selecting a Drive for Your Stepper Motor >

To get the most out of your stepper motor, you need to pair it with the proper drive. There are three critical elements to keep in mind when making your selection: voltage, current and inductance. Each one plays an important part in a motor’s…

The Big Debate – Stepper vs Servo >

What is the best motor technology to use in a motion control application? There are numerous technologies to create motion, from hydraulic to pneumatic or electromechanical. In the world of precision motion control, many machine designers face a…
Kollmorgen stepper motor

How to Select a Stepper Motor >

Knowing how to selct a stepper motor is critical for optimal performance. Use our speedy, dependable Stepper Optimizer tool for precise selection.

How Does a Stepper Motor Work? >

A stepper motor is a simple two phase brushless synchronous motor containing a segmented magnetized rotor and a stator consisting of a prescribed number of electromagnetic coils. When energized, these coils create north and south polls that push or…

Motor Derating Due To High Ambient Temperatures >

How do I calculate a motor’s continuous torque when it is operating in an environment above its rated temperature? Since the motor’s continuous torque (Tc) is rated in a 40°C ambient, how can I estimate the motor’s continuous torque during my…

Going Small - How Current Step Motor Technology Can Help You Reduce Machine Size >

As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a…

That's One Small Step... 0.9 vs 1.8 Degree Step Angle >

There is a lot of discussion about the 1.8 degree step angle versus 0.9 degree step angle of industrial hybrid stepper motors.  Most stepper motors today have the standard step angle of 1.8 degrees, resulting in a 200 step per…