Skip to main content
blog | Overcoming the Limitations of Missile Design |
|
2 minute read

Missiles operate in some of the most demanding conditions. They can experience massive heat flux when going through the layers of the earth’s atmosphere and because of the sheer speed that the missile is traveling at. With speeds in excess of 10,000 kilometers per hour, they require components that can provide reliability and precise motion under these conditions. And with the need to respond to higher demands for performance, the technology powering these missiles needs to deliver more torque and power in relation to weight.  

The typical approach to designing a missile to address these conditions is to create a larger motor that can provide the right amount of power while not being affected by high temperatures. However, this causes the missile to have a larger footprint, which takes more space and costs more money. A smaller footprint can mitigate those costs but sacrifice performance.  

The goal is to create a motor that can provide the same performance but in a smaller size, or keep the same footprint but increase performance. Because there’s only so much power to squeeze out of the technical components, looking to other areas surrounding the motor, such as the insulation or magnet material, can provide the right combination to achieve more power in the same space.  

Insulation Systems 

Current motors with a typical insulation system can operate within a 150°C–180°C ambient temperature range. This range limits the operational range of the missile, especially when it comes to hypersonic environments. To get more power out of the motor and sustain it at a higher working temperature, A&D engineers at Kollmorgen turned to material science to identify unique methods of replacing the insulation to increase the ambient temperature range. After testing several materials, the engineers developed recipes for employing different insulation materials to be optimized for specific applications, allowing the motor to operate. These new insulation materials allowed the motor to operate at an elevated level by boosting its continuous operating temperature to 210°C–240°C.

Magnet Material 

The most common magnet material used in commercial applications is neodymium iron boron (commonly referred to as NEO magnets). These NEO magnets perform well in everyday applications, but when they are subjected to the extreme temperatures found in missile applications, their performance starts to deteriorate. Like copper insulation, this limited the overall performance of the motor and missile. But through pioneering material science research, a different alloy to solve the extreme temperature limitations was identified: samarium cobalt. They are similar in strength to NEO magnets but have a higher temperature rating and coercivity with maximum usage rating of 320°C. Using this magnet allows for greater power without the impact of increased temperature.  

Continued Innovations in Material Science 

Kollmorgen has long been a leading expert in material science and the value it can provide to motor performance and innovation. However, it goes beyond simply understanding material science and extends to testing and validating a material’s performance capabilities. Kollmorgen has spent literally thousands of hours identifying, testing and refining materials. And that’s just for the prototype. Changing materials has implications for the manufacturing process, where Kollmorgen has the expertise to deliver these innovations at scale.  

As a partner that works to mitigate risk throughout the supply chain, Kollmorgen constantly pushes the edge of material science and understands its key role in improving the performance and value of motors. Through constant innovation, we can take these discoveries and apply the benefits to real-world aerospace and defense applications. 

Ready to see where material science can take you? Let’s get started. Consult a Motion Expert.

Consult an Expert

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Driving Aerospace & Defense Innovation with Motion Technology >

Motion technology is the execution layer that turns AI and software into physical mission readiness. Explore how it drives aerospace and defense innovation at scale.
Space satellite

Engineering Motion Systems for Space: A Guide to Reliability, Scalability and Mission Success >

Move from terrestrial prototypes to mission success with a practical guide on evaluating space-ready motors and engineering spacecraft motion control.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles

Designing Motion Control for Turrets and Large Azimuth Drive Systems in Military Ground Vehicles >

It’s important to distinguish between technology and topology when designing motion systems for large military ground vehicles. Topology is the high-level architecture of how those components are arranged and interact within your system.
Motion Design for Next-Generation Armored Fighting Vehicles

Motion Design for Next-Generation Armored Fighting Vehicles >

Learn what to consider when designing for next-gen armored fighting vehicles, from electromechanical motion architectures to mission-critical performance.
Technology vs. Topology: Designing Motion for Turrets and Large Azimuth Drive Systems

Technology vs. Topology: Designing Motion for Turrets and Large Azimuth Drive Systems >

Learn how to select the right motion system topology for your ground vehicle platform and go from concept to combat success with Kollmorgen.
Enhance Defense System Development with Advanced Motion Design

Enhance Defense System Development with Advanced Motion Design (Turkey) >

Optimizing the form factor and ensuring the reliable function of your defense system design is crucial. As you think about your design, Kollmorgen and its partner brands under the Regal Rexnord banner can help you build success by delivering…
Enhance Missile Development with Advanced Motion Design

Enhance Missile Development with Advanced Motion Design >

This webinar will discuss the critical motion control elements needed for effective missile development and how these elements can work effectively together — from motors of all sizes to ball screws, resolvers, brakes, bearings and seals, to…
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…