Skip to main content
blog | What You Need to Know When Selecting a Drive for Your Stepper Motor |
|
2 minute read

Designed to deliver peak torque in open-loop systems, such as applying labels to bottles on a high-speed conveyor system, stepper motors are a great choice for achieving optimal results at an affordable cost. But having done your research and chosen a stepper for your application, there’s still the other half of the motion system to consider.

To get the most out of your stepper motor, you need to pair it with the proper drive. There are three critical elements to keep in mind when making your selection: voltage, current and inductance. Each one plays an important part in a motor’s performance, and not accounting for these parameters can lead to poor performance or even cause the motor to overheat and fail—resulting in lost production time and increased maintenance costs. 

Voltage Rating

Exceeding the motor's maximum rated voltage, or sometimes operating at higher supply voltages, can cause the motor to fail. That’s why when choosing a drive for a stepper motor, you need to know the motor's maximum rated voltage or typical rated voltages from catalog data or performance curves. Stepper motors are typically powered by drives operating on AC power, either 120 or 240 volts, or low-voltage DC power, such as 24, 36 or 48 volts. If you run a motor at a higher voltage than specified, such as running a motor designed for 24 volts DC at high voltage, it will quickly overheat. Conversely, running a motor at too low of a voltage, such as a high-voltage motor run at 24 volts DC, will produce less power, and if the load isn’t reduced this could cause the motor to stall.

When it comes to finding a motor’s rated voltage listed on the nameplate, it can sometimes be hit or miss. Never take a blind gamble on the drive. Instead, if the voltage information isn’t shown on the motor, you should consult the catalog or ask the manufacturer directly. Some manufacturers offer online design tools that allow you to create performance curves for stepper motors based upon the available voltage and current in your application. By using those same specifications, voltage and current, the tool will also output a temperature versus speed curve that will show you if you might overheat the motor.

Current Rating

When selecting a drive, you want one that can deliver the right amount of current to the motor. Current matching isn’t necessarily needed, but running at a lower current will produce lower torque. If the load isn’t reduced, this can cause the motor to stall. Setting the drive current higher than the current rating of the motor will cause the motor windings to overheat and fail. This will cause permanent damage to the motor. Whether it is a software setting or DIP switch setting, you’ll want to select the current rating that most closely matches the current rating for the motor.

Inductance

Each motor has a winding inductance, and drives typically have an inductance range that needs to be considered when pairing the motor. Therefore, you’ll need to know the inductance of the motor and pick a drive that is compatible with the motor. Depending on the supply voltage, if a motor inductance is too high, the motor current cannot be delivered in the required time. If it is too low, then current is given too fast to the motor, causing the drive to potentially overheat and fail. And if the inductance is higher than an applicable motor inductance range for the drive, it might not turn at all.

Consult an Expert

P8000 Stepper Drive

New, more compact drives offer greater smoothness, precision and torque density for fixed-load, low-speed, point-to-point applications

Learn More

PMX Series

The PMX family of hybrid stepper motors offers unmatched versatility through a wide range of standard and customizable options, unmatched value through exceptional performance at an affordable cost, and unmatched reliability through Kollmorgen’s superior motion expertise and build quality.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

5 Mistakes to Avoid When Specifying a Stepper System

5 Mistakes to Avoid When Specifying a Stepper System  >

Stepper systems can be efficient, powerful and quiet — but only if you get it right. When specifying stepper motors and drives, here are 5 common mistakes to avoid and 5 best practices to implement, speeding your development of a successful machine.

Expand Machine Capability with Programmable Stepper Drives  >

Discover the future of stepper drives. Join us as we explore advanced, software-programmable ​stepper ​solutions in this new online webinar.

Kollmorgen Stepper Motor Catalog >

Kollmorgen’s stepper motors are designed with versatility, ease–of–use, and cost-effectiveness in mind. They provide high torque in a small package and come in a wide range of standard sizes, constructions, windings and options.

POWERMAX II® M and P Series Stepper Motor Catalog >

The POWERMAX II® M and P series is ideally suited for lower loads and designed to provide exceptional value, versatility and ease of use. Among the most powerful stepper motors available, they deliver high torque in a compact package and are…

POWERPAC® K/N Series Stepper Motor Catalog >

The K/N series are larger step motors with the power, rugged construction, and options that make these motors ideal for heavy industrial applications. Options include: IP65, terminal boxes and MS connectors. Enhanced versions provide the maximum…

P8000 Stepper Drive Family Brochure >

As Kollmorgen’s flagship stepper drive platform, the P8000 family delivers advanced functionality, expanded output and greater compatibility.

Get Exact Positioning Without the Complexity with Stepper Motors >

If you’re looking for precise motion with easy setup, then stepper motors should be your first choice when building or upgrading a machine.

Why Does My Stepper Motor Get Hot? >

All electric motors heat up during operation, which is simply a product of passing current through a coil of wire. Electric motors use copper wire to form coils that are part of the electromagnetic circuit required to produce rotation. While copper…
Diagnostic Imaging: Motion for Every Modality

Diagnostic Imaging: Motion for Every Modality >

An aging population, a growing burden of disease, continuous development of new clinical applications, and global advancements in the standards of disease prevention, early detection, diagnosis and treatment. For all these reasons and more,…