Skip to main content
blog | The multi-talent in automation |
|
2 minute read

The electronics engineer A. M. Barrett Jr. invented the first automated guided vehicle in the 1950s. Today, automated guided vehicles bring value to the most shifting applications.

Intralogistics purposes

Automated guided vehicles improve efficiency, safety and quality in manufacturing and warehousing processes. In manufacturing, typical applications are line to storage, material to line, inventory moves, line production and movement of material between production cells. Moving on to warehousing, automated guided vehicles are used for picking, shipping and receiving, replenishment, dispatch and cross-docking.

When moving heavy goods, such as within the ceramics/tiles and paper/printing industries, automated guided vehicles have been commonly used for decades. You also find these vehicles in other types of factories (electronics, food, metal, mining, tire) as well as in hospitals and pharmaceutical production. Thanks to precise and safe movements, they also contribute to reduced physical damage and personal injuries.

The perfect kickstart

Industry 4.0 is on everybody’s lips right now – for good reason. Linking the whole value chain digitally will allow us to produce and move things faster and safer at a higher level of quality. There is only one catch: Where do I start?

The multi-talent in automationAutomated guided vehicles, based on Kollmorgen’s NDC Solutions platform, give customers a flying start into industry 4.0. The platform is flexible, well-proven and offers a payback time usually as little as 1-2 years. A reasonable initial investment makes the buying decision easier for management.

The annual production of automated guided vehicles has grown rapidly in recent years. With the industry 4.0 revolution underway and a booming e-commerce sector not least in China, the future of our NDC Solutions platform looks bright.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…