Skip to main content
blog | Speeding up installation of smart mobile robots |
|
2 minute read

Speeding up installation of smart mobile robots

What if you could cut the installation time of smart mobile robots by up to 25 percent? This is now reality with new software for NDC Solutions from Kollmorgen. One tool for all layout fine-tuning and an automated verification process to secure quality save lots of time even for the experienced application engineer. 

Disruptive approach

With a growing number of smart factories and smart warehouses around the world, the need for fast installation of smart mobile robots is bigger than ever. The trend is the same for other automated vehicles such as AGVs, carts and tuggers. But finding new ways to cut time is not a new challenge in the vehicle automation industry. The team at Kollmorgen had to think beyond the ordinary.

“Our primary focus was to develop new software that could cut the time it takes to do an installation,” says Peter Bladh, Director Product Management & Marketing at Kollmorgen. “Smart functionality guides the application engineer through the process, ensuring efficient use of valuable engineering time and system quality.”

Removing the repetitive

The new software makes it easier to find layout information and the application engineer no longer has to swap between different tools to perform different layout tasks. All verification reports of the physical layout and finalized project steps are generated automatically.

The goal for Kollmorgen is software that can reduce the installation time by up to 90 percent compared with today.

How much time can you save?

Let’s say that you are dealing with an application project of 300 hours, where 160 hours are spent on site. Removing 25 percent of the installation time saves you 40 hours (160 x 0.25) of work, that is, a full working week. Five projects per year mean you save some 200 hours.

Check out this video for more information on how new software can contribute to shorter and safer mobile robot installations in smart factories and warehouses. Make sure you stay on top of this topic by subscribing to our newsletter and feel free to contact us or any of our partners around the world.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…