Skip to main content
blog | How Does a Direct Drive Linear Servo Motor (Actuator) Work? |
|
2 minute read

A direct drive linear actuator, using a permanent magnet linear servo motor produces force and velocity based on the supplied current and voltage and provides a linear movement along the axis being driven. The linear servo motor works as part of a closed loop system providing force and velocity as commanded from a servo controller utilizing feedback to close the loop. In simple terms, a linear servo motor behaves identically as a rotary servo motor – it’s just rolled out flat and straight. Various feedback elements in the system supply information such as current, velocity, or position of the motor coil to the servo controller, which adjusts the motor action depending on the commanded parameters. A linear servo motor is a direct drive solution where the load is directly connected to the moving portion of the motor.

Direct drive linear motors are available in a variety of configurations (iron core, U-channel, tubular) but ultimately work the same. The direct drive linear actuator is part of a servo mechanism consisting of five key elements – a coil or forcer, a magnet way or magnetic shaft, a feedback device, mechanical elements consisting of linear bearings and supports, and driven by a servo drive or controller. The feedback device is typically a linear scale such as a linear encoder or transducer or can be other devices such as a potentiometer, Hall-effect device, tachometer, LVDT, or any other sensor as appropriate. The mechanical elements guide the forcer or coil along the magnet way, maintaining the proper air gap between the coil and magnets. Completing the servo system is the control electronics that powers the motor and compares the feedback data and command reference to verify that the linear servo motor is operating as commanded. There are many types of direct drive linear motor applications from simple X-Y stages to complex gantry systems - such as multi-axis laser cutting machines driven by complex motion controllers.

Similar to our blog on how a servo motor works, multiple embedded servo loops are tuned for optimal performance to provide precision motion control. The system consists of current, velocity, and position loops that utilize precision feedback elements. Each loop signals the subsequent loop and monitors the appropriate feedback elements to make real time corrections to match the commanded parameters.

The base loop is the current or force loop. Current is proportional to force in a linear servo motor, which provides acceleration or thrust. A current sensor is the device that provides feedback related to the current flowing through the motor. The sensor sends a signal back to the control electronics - typically an analog or digital signal proportional to the motor current. This signal is subtracted from the commanded signal. When the servo motor is at the commanded current, the loop will be satisfied until the current drops below the commanded current. The loop will then increase current until the commanded current is reached, with the cycle continuing at sub second update rates.

The velocity loop works in the same fashion with voltage proportional to velocity. The velocity loop sends the current loop a command to increase current (thus increasing voltage) when the velocity falls below the commanded velocity.

The position loop accepts a command from a PLC or motion controller which, in turn, provides a velocity command that is fed to the velocity loop which, in turn, commands the required current to accelerate, maintain, and decelerate the motor to move to the commanded position. All three loops work in optimized synchrony to provide smooth and precise control of the direct drive linear servo motor.

Consult an Expert

Direct Drive Linear Motors

Using Kollmorgen DDL direct drive linear motors, your machine can be simpler, faster, more precise and reliable. Pair your ironless, low profile or ironcore linear motor with an AKD or AKD2G servo drive for industry-leading power density.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights >

IC Ironcore DDL linear motors and AKD servo drives delivered 65% greater positioning accuracy and 15% higher productivity for this double-faced grinding machine.

Kollmorgen introduces new high-voltage IC Ironcore DDL direct drive linear motor >

Discover Kollmorgen’s new linear direct drive motor, engineered to move heavy loads with fast precision and to simplify machine design for the global marketplace.
Direct Drive Linear Technology Enables Large-Scale Production of Calcium-Titanium Ore Solar Cells

Direct Drive Linear Technology Enables Large-Scale Production of Calcium-Titanium Ore Solar Cells >

Learn how a major solar-cell manufacturer significantly increased productivity and quality using high-performance, zero-cogging IL Ironless DDL direct drive motors.
Incorporating a Direct Drive Linear Motor into Your High Performance Machine

Incorporating a Direct Drive Linear Motor into Your High Performance Machine >

When mechanical designers use conventional servo motors to drive ballscrews or rollerscrews for linear motion, they quickly encounter limits to the speed and precision they can attain. Direct drive linear motors provide substantially higher…
Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production >

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Cartridge DDR

Going Beyond Performance: Cost Savings with Direct-Drive Systems >

The performance benefits of direct-drive motors are well documented: industry-leading performance, improved accuracy, higher throughput, better reliability and quieter operations. This is because, unlike a conventional motion setup, a direct-drive…

Reducing Defects while Improving ROI in Metal Stamping with Direct-Drive Technology >

Compared to mechanical and hydraulic presses, mechanical servo metal stamping presses use high torque brushless motors to create more complicated stampings at faster speeds. But the type of motors used—a traditional geared or chain drive system or a…

Kollmorgen Is on the Perseverance Rover—And Extreme Environments Everywhere >

From the surface of Mars to the depths of the ocean, from the core of the earth to the core of the human body, Kollmorgen motion systems take on the most extreme environments.

Tips on How to Confidently Set Up Your Linear Motor System >

Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications.  In order to achieve the highest level of performance, the linear motor system must be commissioned…