Skip to main content
blog | Catch the future while you can |
|
2 minute read

Catch the future while you can

Industry 4.0, the fourth industrial revolution, is changing the way materials and information move in factories. It is happening now in all types of businesses around the globe. A paradigm shift that is not only creating a lot of opportunities, but also a lot of stress for decision makers. Where do you need to invest, in what and when? Smart mobile robots give you a flying start.

Smart factories

The first industrial robot was sold in 1961 to General Motors. It was designed to transfer parts from one point to another in one of their factories. A big leap forward at the time and since the 1960s, robotic arms have been a natural part of the automotive industry as well as many other industries.

Today we talk about smart factories, in line with the industry 4.0 concept. Humans work alongside industrial robots, so-called cobots, and data is transferred seamlessly through all kinds of systems. Smart mobile robots, such as Comau Agile1500, are gaining ground as they can move materials swiftly between the workstations. The smart factory is open, agile and always ready to produce and deliver what customers want.

Controlled freedom

Smart movement of materials is a key ingredient in a smart factory. Recently, Kollmorgen introduced natural navigation for automated guided vehicles (AGVs) including mobile robots, self-driving vehicles and carts. Natural navigation allows the vehicle to navigate using objects in the environment instead of reflectors or markers. The workstations can be placed anywhere, and they can be re-arranged easily.

But what about traffic rules? A classic AGV challenge, growing with the number of vehicles, where you want to avoid traffic jams without losing too much flexibility. The latest system software from Kollmorgen uses advanced algorithms for planning traffic, saving time during start-up and when making changes. Combined with natural navigation, this means that the vehicles are always free to take the smartest path to the next station.

No time to lose

The fourth industrial revolution is here to stay. Demands from customers on delivery times and quality will just continue to rise in a more global world. Smart mobile robots will not be the answer to all your industry 4.0 challenges, but to a surprising number of them. You are up and running relatively fast and the payback period is often as low as 1-2 years.

Some years from now, people will travel to work in driverless vehicles. Is it realistic to think that they will still be working as forklift truck drivers? Catch the future while you can. Start your journey to a smart factory by reading more about industry 4.0 or contact us or any of our partners directly. Subscribing to this newsletter is also an excellent way to stay updated.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…