Search Articles
| Changing the Com Port Number for a USB to Serial ConverterMost laptops do not have a 9-pin serial port. So we are forced to use USB to Serial converters or adapters for communicating with devices over RS-232. Most older GUI software only allows the selection of the lower numbered com ports, such as COM1, COM2, COM3, and COM4. | inglês | |
| PiCPro Programming SoftwareA Single-Point Solution for Total Machine Control PiCPro® offers the most flexible toolset for motion application programming available. Motion instructions are as simple to use as ladder logic counters and timers. | inglês | |
| Commissioning of Unknown Hall Motors with the S300Commissioning of Unknown Hall Motors with the S300 Find out the hall counting direction HALLDIR MPOL | inglês | |
| Linear Encoder Supported by AKD, S700, and S300List of known linear encoder supported by AKD / S700 / S300. | inglês | |
| User Units in the PDMM Table of Contents PLCOpen Motion Engine: Setting User Units | inglês | |
| Comissioning of Hall onlyHall-ONLY as a Feedback in S300/S700 Drives: Hall-ONLY as a Feedback has some specific characteristics. This document aims to enhance the comprehension of Hall-ONLY. | inglês | |
| Functional Safety with AKD Table of Contents Safety Comparison Stop | inglês | |
| Supported Linear Feedback Devices for AKD / S300 / S700In order to support linear motors the following linear feedback devices have been tested with our drives: | inglês | |
| Using EOT (End of Travel) hardware limit switches in a KAS applicationThe PDMM consist of a control card and a drive card. The controller card contains the application program and the drive card contains the servo loops. | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >