Search Articles
| AKD 48A - Low Inrush Current of 4AThe high voltage drive uses a "pre-charge" circuit to load the bus capacitors. (The total resistance is 160 ohms). With a incoming power supply of 480VAC, being switched on right at the voltage peak, we have: | inglês | |
| Hall Sensor Alignment ProcessHall Effect Sensors are used to establish proper motor commutation on Brushless Servo motors. To be effective, the Hall Effect Sensors must be properly aligned with the servo motors phases. Motor manufacturers typically align the Hall sensors at the factory so customers do not ne | inglês | |
| Rehoming in a Pipe Network applicationRehoming in a KAS Pipe Network application | inglês | |
| AKD DC Bus Link Creating n521 (Regen Over Power) Warning?Using the AKD's DC bus link to share bus voltage across a series of drives is a good way to limit regen needs and unnecessary energy costs. | inglês | |
| AKD GSDML FilesAKD and AKD2G Profinet GSDML file location | inglês | |
| Part Numbers for AKD-N Amphenol ConnectorsThe followng table provides the Kollmorgen part numbers for the feedback connectors which are used to connect to the A | inglês | |
| Save Variable Values to the PCMM/PDMM's Internal Flash or SD card MemoryThe attached sample .kas project contains a program (SaveVarsToFlash) that stores application variables into a .csv file located on the PCMM/PDMM's internal FLASH memory or removable SD card. Steps to accomplish this wih FLASH memory are: | inglês | |
| Save Variable Values to PDMM SD memoryThe attached sample .kas project contains a program (SaveVarsToSDcard) that stores application variables in a .csv file on the PDMM SD card: | inglês | |
| Loading and saving application parameters (recipes) to NVRAM memory. Saving recipes to PCMM or PDMM memory. | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >