Search Articles
| Permanent Magnet Servomotor and Induction Motor ConsiderationsMotion long considered a mainstay of induction motors, encroachment in the area of 50 hp and greater have been seen recently for some applications by permanent magnet (PM) servomotors. | inglês | |
| How does a multi-turn encoder function, including roll-over?Absolute multiturn encoder rollover | inglês | |
| Recommendations on replacing the Cimrex41 HMI panels?The Cimrex 41 operator terminal (M.1302.74250 is obsolete and replaced by EXTER T40m (M.3000.0170) or T40t (M.3000.0171). | inglês | |
| What do I do if I encounter an F305 Fault (Brake Open Circuit) on my AKD servo drive?F305 and MOTOR.BRAKE | inglês | |
| I'm getting an F401 Error on the AKD Servo DriveThe F401 error results when parameters related to the anticipated feedback device are in error. | inglês | |
| Problems connecting a CompactLogix PLC to an AKD drive?When connecting an AKD to a CompactLogix PLC (or any PLC that communicates via EtherNet/IP), please make certain you are using an AKD version which supports EtherNet/IP Fieldbus communications. | inglês | |
| Velocity mode control of an axis with KAS controllerThe attached demo project shows how to control a servo axis with a KAS controller in Velocity Mode instead fo the default Position Mode. | inglês | |
| Creating a Motion Task S-Curve Profile Table in the AKDUse the Excel file titled “AKD S-CURVE GENERATOR TWO.xls” (see attachment) to generate a csv file with the profile data. | inglês | |
| Does KAS IDE work on Windows 10?KAS IDE supported by Windows 10. | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >