Skip to main content

Kollmorgen Support Network

How does a multi-turn encoder function, including roll-over? | 30 Mar 2016 | |

How does a multi-turn encoder function, including roll-over?

Endat and BiSS multi-turn encoders use a second encoder disc that is geared to the primary disc.  The multi-turn disc will turn one line for each revolution of the motor/encoder.  The muti-turn data will roll over at 2048 revs from absolute zero.  The full range between roll-overs is -2048 revs to zero to +2048 revs.  When the motor passes the roll-over point, the drive will continue counting the feedback position as normal.  But when the drive is power cycled, the position will be read from the encoder as it is in the new value range. 

See FB1.EXTENDEDMULTITURN for tracking the multiturn rollovers and retaining the correct absolute position through power cycles.

About this Article

Mark.Duckwitz