KAS IDE v4.00 is now available!!New Features
Next Generation Controller Software
Compatible with PCMM/PDMM (1st Generation Controllers)
64-bit Runtime (2nd Generation Controllers)
AKD2G Modular Device Profile (MDP) I/O
MDP IO support for model variants
First AKD2G TuningUsers facing the tuning of an AKD2G servodrive for the first time will have to use the Workbench configuration software tool which, for novice users or users of the Servostar series drive, may confuse them given the difference in the graphical interface and the many features introduced. This note…
inglês
(ABM)(Desenhos 3D) Altra Brasil Servo SeriesEsses modelos 3D destinam-se a orientar suas atividades de projeto e podem ser usados como informações de referência. Certifique-se de consultar um especialista da Kollmorgen para garantir que você tenha as informações mais atuais e precisas para os aspectos críticos do trabalho de design.
Portuguese, Brazil
AKD2G Actions Used for AC Mains Switch-Off after Controlled StopThe controlled motion of any given axis of a machine will require the AC mains to be dropped after completion of an emergency-stop (NEC - Category 1). The necessary NEC stop category is determined based on the machine builder’s safety audit. This application note is only valid for Stop…
inglês
AKD2G - Sending Secondary Feedback through EtherCATThe AKD2G's various feedback options allow for incorporating up to 5 feedback devices into the drive. Occasionally the feedback is not used for servo AXIS control (a position used as a direct command or feedback to a servo axis) but used as an additional or axillary feedback signal for the motion/…
inglês
AKD2G Gantry Mode with KAS ControllerAKD2G Dual Axis drives have the ability to use the new Gantry Command Source. When the Command Source is changed to 4 - Gantry, Axis2 will follow all commands sent to Axis1 (enable/disable and motion commands).
inglês
(ABD & ABM) Altra Brasil Servo SeriesAs séries ABD® (Altra Brasil Drive) e ABM® (Altra Brasil Motor) oferecem uma linha completa de servo-acionamentos com base nas tecnologias EtherCAT e Analógico, desenvolvida sob medida para atender às demandas do mercado brasileiro.