Search Articles
| Encoder connector Motor View Contact socket Contacts Lamella Clamp Dimensions | inglês | |
| Power Connector Motor M40, 6-poles View Contact socket Contacts Lamella Clamp Dimensions | inglês | |
| AKD Feedback Connector | inglês | |
| AKD Power Connector Used with AKD, voltage type 06, current types 3A and 6A | inglês | |
| Holding Brake Valid for AKM, AKMH The AKM holding brakes are designed as standstill brakes and are not suited for repeated operational braking. Built-in holding brakes without further equipment must not be used to ensure personnel safety. | inglês | |
| Power Connector Motor M40, 8-poles View Contact Socket Contacts Lamella Clamp D | inglês | |
| Commissioning AKD The following provides brief explanations of the most important points for AKD commissioning and also goes into more detail on the key issues which need to be taken into account: Basic settings of the AKD Before the first controller parameters are set, the parameters should first be reset to… | inglês | |
| Safety Concept AKD Table of Contents About the "Safe Torque Off "(STO) Function | inglês | |
| Hybrid Connector Washdown Motor M23 View Contact Socket Contacts Lamella Clamp Dimensions | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >