TwinCAT 3 To AKD2G EtherCAT Setup and DemonstrationThe attached video covers important topics such as ESI (XML) file acquisition and importation into TwinCAT 3. Basic setup and motion from the TwinCAT 3 console are also demonstrated. Finally how to recognize and resolve a mismatch between the Device Description (ESI) and the physic
Mean Time Between Failure AKD AKM Gen 1Summary of Juran's Mean Time Between Failure (MTBF) for AKD & AKM. Data up through 2014.
Purpose
A rough calculation of the Mean Time Between Failure (MTBF) based on historical data. This tool is to be used at a customer's request. MTBF is not "operating life" or "service life".
inglês
Sizing AKT Remote IO AKD-PDMM controller/drive, AKD, AKD2G, and S700 drives, and PCMM standalone controller all contain hardware I/O that can be used in an application to interface to other control elements on the machine. Typically, to minimize overall system cost, IO point on these products are used first…
inglês
PC and KAS UDP communication: C# example (Visual Studio Express 2013)This example shows how to exchange data between a PCMM or AKD PDMM and a PC using UDP.
The attached KAS program works with the target controller and 2 AKD drives.
The PC-based program is written in C# and receives the axis positions from the controller. It is also possible to…
inglês
KVB Alarms Video - Creating And Using Them With AKI HMI PanelsKollmorgen Visualization Builder (KVB) software has built in alarm features. Users can easily determine when certain values of tags will raise alarms, how they are displayed on the HMI, how they can be cleared, how users can view a history of past alarms, and if text messages or emails should be…
Reação a situações de falha S300-S700Válido para S300, S700
Dependendo do problema atual, as falhas são gerenciadas de forma diferente (diferentes níveis de erro):