KAS Project Backup and Restore
This video demonstrates:
- Backing up a KAS system to the Controller’s SD card
- Exporting this backup to one system file on a PC
- Importing a system file and converting back to multiple files on the SD card
- Restoring the system configuration from the SD card to the KAS System hardware
Backing Up and Restoring a KAS system facilitates:
- Having a backup of the Controller and Drives in the KAS system
- Duplicating the system configuration onto additional machines
- Updating or loading a part of a KAS system, for example a particular drive in the system
There are 2 methods to back up and restore a KAS System
- Using the B2/B3 buttons on the controller’s front face
- Using the Webserver inside IDE software or directly in an internet browser
- With the B2/B3 method the controller configuration can be backed up and restored
- With the Webserver method in addition to the controller, the Ethercat Configuration and Drives can be backed up and restored
Loading...
Home >
Knowledge Base >
FAQs >
Downloads >