Skip to main content

Kollmorgen Support Network

KVB Alarms Video - Creating And Using Them With AKI HMI Panels | 17 Sep 2020 | |

KVB Alarms Video - Creating And Using Them With AKI HMI Panels

Kollmorgen Visualization Builder (KVB) software has built in alarm features. Users can easily determine when certain values of tags will raise alarms, how they are displayed on the HMI, how they can be cleared, how users can view a history of past alarms, and if text messages or emails should be sent along with certain alarms. The video embedded below goes through the basics of setting alarms and options for how they are viewed on Kollmorgen AKI HMI panels.

Loading

About this Article

Joe Parks