Pular para o conteúdo principal

Search Articles

TwinCAT 3 To AKD2G EtherCAT Setup and DemonstrationThe attached video covers important topics such as ESI (XML) file acquisition and importation into TwinCAT 3. Basic setup and motion from the TwinCAT 3 console are also demonstrated. Finally how to recognize and resolve a mismatch between the Device Description (ESI) and the physic inglês
Reading of AKD axes position by Python and Raspberry Pi 3 Modell BThis solution allows you to read the motor positions of three AKD axes using Raspberry Pi hardware and Modbus TCP/IP. inglês
AKD2G Low Voltage DC Operation Table of Contents Overview inglês
Mean Time Between Failure AKD AKM Gen 1Summary of Juran's Mean Time Between Failure (MTBF) for AKD & AKM.  Data up through 2014. Purpose A rough calculation of the Mean Time Between Failure (MTBF) based on historical data. This tool is to be used at a customer's request. MTBF is not "operating life" or "service life". inglês
Sizing AKT Remote IO AKD-PDMM controller/drive, AKD, AKD2G, and S700 drives, and PCMM standalone controller all contain hardware I/O that can be used in an application to interface to other control elements on the machine. Typically, to minimize overall system cost, IO point on these products are used first… inglês
PC and KAS UDP communication: C# example (Visual Studio Express 2013)This example shows how to exchange data between a PCMM or AKD PDMM and a PC using UDP. The attached KAS program works with the target controller and 2 AKD drives.  The PC-based program is written in C# and receives the axis positions from the controller. It is also possible to… inglês
KAS Project Backup and RestoreThis video demonstrates: inglês
Reação a situações de falha S300-S700Válido para S300, S700 Dependendo do problema atual, as falhas são gerenciadas de forma diferente (diferentes níveis de erro): Portuguese, Brazil
Servo drive da série S700 com falha F23Caso a comunicação CANopen não esteja sendo utilizada, utilize este procedimento para desativar a falha F23. Portuguese, Brazil